I am using an LS1021A-TWR board and need to provide 1 PPS external trigger signal.
Referred to 8.7.7.2 External trigger signal from LSSDK 21.08, but I am still not getting the data in fifo. It talks about proper RCW settings to enable this. This is RCW from the bootup logs from the device:
Reset Configuration Word (RCW):
00000000: 0608000c 00000000 00000000 00000000
00000010: 30000000 00007900 60040a00 21046000
00000020: 00000000 00000000 00000000 18000000
00000030: 00080000 891b7340 00000000 00000000
Can someone please confirm if this is correct. If not what should be the correct RCW configuration and how to update the same.
Thanks