LS1021A-TWR - No ethernet devices under linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1021A-TWR - No ethernet devices under linux

495 次查看
z_v
Contributor I

Hello,

I built kernel 4.1.13 for LS1021A and ran it on the TWR. 

The root file system is busybox and the dtb is identical to the one used in Yocto project provided by NXP.

Under u-boot, all 3 ethernet devices work fine. 

Under linux, I can see only the "lo" device.

Is there any component I should add to the linux configuration ?

The 4.1.13 is a vanilla kernel from kernel.org patched so I can run:

make ls1021a_defconfig 

Thank you,

Z.V

标签 (1)
标记 (1)
0 项奖励
0 回复数