LS1021A-TWR: Full reprogram

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A-TWR: Full reprogram

763件の閲覧回数
z_v
Contributor I

Hello,

In order to reprogram the original image I did the following:

SW2 - 01001111

SW3 - 01100101

(This is setup I got here)

But in CW I got the message:

Error: The algorithm was not able to run on the target of the flash is not configured properly

Error: Getting flash ID failed

Can you please help ?

Both banks are currently not running.

Thank you,

Z.V

ラベル(1)
タグ(1)
0 件の賞賛
2 返答(返信)

651件の閲覧回数
z_v
Contributor I

Hello,

I recreated the CW RAM application project.

Now programming works fine.

Thank you !

Z.V

0 件の賞賛

651件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which exactly TWR revision is in question?

Please provide photos of the on-board inscriptions and stickers.

Please provide additional information about CodeWarrior setup:

1) which Debug Configuration is used?

2) complete Flash Programmer log as a text file

0 件の賞賛