LS1021A-IOT connection to the network

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A-IOT connection to the network

2,124件の閲覧回数
victormazin
Contributor II

Hi,

We use the LS1021A-IOT reference board and try to connect the board to our network.

When I connect the Ethernet cable between  the board socket ETH0 and a network router the IP address does not adapt automatically.

What should I do to connect the LS1021A-IOT board to the network?

 

I verified the /etc/network/interfaces setting. Please see below. I also attached the log file.

 

Regards

Victor

root@OpenWrt:/# ifconfig

br-lan    Link encap:Ethernet  HWaddr 00:1f:7b:63:02:6d 

          inet addr:192.168.1.1  Bcast:192.168.1.255  Mask:255.255.255.0

          inet6 addr: fd5b:6a49:e38a::1/60 Scope:Global

          inet6 addr: fe80::21f:7bff:fe63:26d/64 Scope:Link

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:261 errors:0 dropped:0 overruns:0 frame:0

          TX packets:163 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:21823 (21.3 KiB)  TX bytes:12790 (12.4 KiB)

 

 

eth0      Link encap:Ethernet  HWaddr 00:1f:7b:63:02:6d 

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:291 errors:0 dropped:0 overruns:0 frame:2

          TX packets:156 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:33186 (32.4 KiB)  TX bytes:12068 (11.7 KiB)

          Base address:0xc000

 

 

lo        Link encap:Local Loopback 

          inet addr:127.0.0.1  Mask:255.0.0.0

          inet6 addr: ::1/128 Scope:Host

          UP LOOPBACK RUNNING  MTU:65536  Metric:1

          RX packets:1306 errors:0 dropped:0 overruns:0 frame:0

          TX packets:1306 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:90396 (88.2 KiB)  TX bytes:90396 (88.2 KiB)

 

 

root@OpenWrt:/# cat /etc/network/interfaces

# /etc/network/interfaces -- configuration file for ifup(8), ifdown(8)

 

# The loopback interface

auto lo

iface lo inet loopback

 

 

# Wireless interfaces

iface wlan0 inet dhcp

        wireless_mode managed

        wireless_essid any

        wpa-driver wext

        wpa-conf /etc/wpa_supplicant.conf

 

 

iface atml0 inet dhcp

 

 

# Wired or wireless interfaces

auto eth0

iface eth0 inet dhcp

iface eth1 inet dhcp

 

 

# Ethernet/RNDIS gadget (g_ether)

# ... or on host side, usbnet and random hwaddr

iface usb0 inet static

        address 192.168.7.2

        netmask 255.255.255.0

        network 192.168.7.0

        gateway 192.168.7.1

 

 

# Bluetooth networking

iface bnep0 inet dhcp

 

 

root@OpenWrt:/#

Original Attachment has been moved to: network.txt.zip

ラベル(1)
0 件の賞賛
返信
1 返信

1,769件の閲覧回数
Pavel
NXP Employee
NXP Employee

Enable DHCP support using kernel menu. See attachment.

Use udhcpc utility for starting the DHCP client on your board.

Look at the following pages for adding staring the udhcpc after boot:

http://manpages.ubuntu.com/manpages/saucy/man5/interfaces.5.html

https://www.opennet.ru/man.shtml?topic=interfaces&category=5&russian=2

http://manpages.debian.org/cgi-bin/man.cgi?query=interfaces&sektion=5&apropos=0&manpath=Debian+5.0+l...


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信