Hi,
We use the LS1021A-IOT reference board and try to connect the board to our network.
When I connect the Ethernet cable between the board socket ETH0 and a network router the IP address does not adapt automatically.
What should I do to connect the LS1021A-IOT board to the network?
I verified the /etc/network/interfaces setting. Please see below. I also attached the log file.
Regards
Victor
root@OpenWrt:/# ifconfig
br-lan Link encap:Ethernet HWaddr 00:1f:7b:63:02:6d
inet addr:192.168.1.1 Bcast:192.168.1.255 Mask:255.255.255.0
inet6 addr: fd5b:6a49:e38a::1/60 Scope:Global
inet6 addr: fe80::21f:7bff:fe63:26d/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:261 errors:0 dropped:0 overruns:0 frame:0
TX packets:163 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:21823 (21.3 KiB) TX bytes:12790 (12.4 KiB)
eth0 Link encap:Ethernet HWaddr 00:1f:7b:63:02:6d
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:291 errors:0 dropped:0 overruns:0 frame:2
TX packets:156 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:33186 (32.4 KiB) TX bytes:12068 (11.7 KiB)
Base address:0xc000
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:1306 errors:0 dropped:0 overruns:0 frame:0
TX packets:1306 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:90396 (88.2 KiB) TX bytes:90396 (88.2 KiB)
root@OpenWrt:/# cat /etc/network/interfaces
# /etc/network/interfaces -- configuration file for ifup(8), ifdown(8)
# The loopback interface
auto lo
iface lo inet loopback
# Wireless interfaces
iface wlan0 inet dhcp
wireless_mode managed
wireless_essid any
wpa-driver wext
wpa-conf /etc/wpa_supplicant.conf
iface atml0 inet dhcp
# Wired or wireless interfaces
auto eth0
iface eth0 inet dhcp
iface eth1 inet dhcp
# Ethernet/RNDIS gadget (g_ether)
# ... or on host side, usbnet and random hwaddr
iface usb0 inet static
address 192.168.7.2
netmask 255.255.255.0
network 192.168.7.0
gateway 192.168.7.1
# Bluetooth networking
iface bnep0 inet dhcp
root@OpenWrt:/#
Original Attachment has been moved to: network.txt.zip