LS1012A TWR boot from SD problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A TWR boot from SD problem

2,773件の閲覧回数
dwokke
Contributor II

Hi all,

So I build a new kernel for the LS1021ATWR board using the QorIQ SDK 1.7. As far as I can tell this has been build without a problem.

Now I want to run the new kernel on the LS1021atwr board via a SD card. For this I followed the manual and copied all files to the SD card, maikng sure the uImage and uImage.dtb are in the boot folder.

Booting the board now hangs almost directly when the SD card is read.

The following shows up in the  terminal on the host.

--------------------------------------------------------------------------------------------------------

U-Boot 2014.01Layerscape-SDK-V1.3+gb7dab7a (Oct 20 2014 - 14:14:11)

CPU:   Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

       00000000: 0608000a 00000000 00000000 00000000

       00000010: 20000000 00407900 e0025a00 21046000

       00000020: 00000000 00000000 00000000 20038000

       00000030: 00000000 881b7540 00000000 00000000

Board: LS1021ATWR

CPLD:  V2.3

PCBA:  V4.0

VBank: 1

I2C:   ready

DRAM:  1 GiB (DDR3, 32-bit, CL=10.5, ECC off)

Using SERDES1 Protocol: 32 (0x20)

Flash: 128 MiB

MMC:   FSL_SDHC: 0

EEPROM: NXID v1

Firmware 'Microcode version 0.0.0 for T1040 r1.0' for 1040 V1.0

QE: uploading microcode 'Microcode for T1040 r1.0'

In:    serial

Out:   serial

Err:   serial

SATA link 0 timeout.

AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode

flags: 64bit ncq pm clo only pmp fbss pio slum part ccc

scanning bus for devices...

Found 0 device(s).

Net:   eTSEC1 is in sgmii mode.

eTSEC2 is in sgmii mode.

eTSEC1 [PRIME], eTSEC2, eTSEC3

Hit any key to stop autoboot:  0

Device: FSL_SDHC

Manufacturer ID: 2

OEM: 544d

Name: SA08G

Tran Speed: 50000000

Rd Block Len: 512

SD version 3.0

High Capacity: Yes

Capacity: 7.2 GiB

Bus Width: 4-bit

3079912 bytes read in 305 ms (9.6 MiB/s)

--------------------------------------------------------------------------------------------------------


Any idea on what I'm doing wrong. SOmething I failed to do first. I'm completely lost as this is my first time using embedded linux.


Best regards,

Dennis

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

1,965件の閲覧回数
dwokke
Contributor II

OK so I found the issue. I tried to build the kernel with CPU freq. Which apparently is not supported by the LS1021A.

My bad!

1,965件の閲覧回数
dwokke
Contributor II

OK so I got a bit futher.

Using the run sdboot command now gives me the following:

------------------------------------------------

=> run sdboot

reading uImage

3079912 bytes read in 154 ms (19.1 MiB/s)

reading ls1021a-twr.dtb

20683 bytes read in 22 ms (918 KiB/s)

reading rootfs

2297001 bytes read in 180 ms (12.2 MiB/s)

## Booting kernel from Legacy Image at 81000000 ...

   Image Name:   Linux-3.12.19-rt30+ls1+g6619b8b

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3079848 Bytes = 2.9 MiB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 88000000 ...

   Image Name:   fsl-image-minimal-ls1021atwr-201

   Image Type:   ARM Linux RAMDisk Image (gzip compressed)

   Data Size:    2296937 Bytes = 2.2 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 8f000000

   Booting using the fdt blob at 0x8f000000

   Loading Kernel Image ... OK

   Loading Ramdisk to becfd000, end bef2dc69 ... OK

   Loading Device Tree to becf4000, end becfc0ca ... OK

Starting kernel ...

-----------------------------------------------------------------------------------

This definitely shows it is reading the SD card with the image I build. However it gets stuck on the starting kernel ...

Any ideas on this?

0 件の賞賛
返信

1,965件の閲覧回数
addiyi
NXP Employee
NXP Employee

I met the same behaviors some times ago and formatting the sd card resolved the problem.

Adrian

0 件の賞賛
返信

1,965件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following page:

http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F6346899.html
 
Do you use similar command sequence for SD Deployment?
0 件の賞賛
返信

1,965件の閲覧回数
addiyi
NXP Employee
NXP Employee

Did you follow the steps from SD Deployment? If, yes, could you share your uboot env (printenv in uboot console).

Adrian

0 件の賞賛
返信

1,965件の閲覧回数
dwokke
Contributor II

Hi Adrian,

Yes I followed the steps from the SD deployment. See the uboot env settings below:

--------------------------------------------------------------

baudrate=115200

bootargs=root=/dev/ram0 rw console=ttyLP0,115200 hdmi high

bootcmd=setenv bootargs root=/dev/mmcblk0p2 rw rootdelay=5 console=$consoledev, $baudrate;mmcinfo;ext2load mmc 0:2 $loadaddr /boot/$bootfile;ext2load mmc 0:2 $fdtaddr /boot/$fdtfile;bootm $loadaddr - $fdtaddr

bootdelay=5

bootfile=uImage

consoledev=ttyLP0

dnsip=10.192.130.201

eth1addr=00:04:9f:03:61:2c

eth2addr=00:04:9f:03:61:2d

ethact=eTSEC1

ethaddr=00:04:9f:03:61:2b

ethprime=eTSEC1

fdt_high=0xcfffffff

fdtfile=uImage.dtb

fileaddr=88000000

filesize=12a

gatewayip=10.192.208.254

initrd_high=0xcfffffff

ipaddr=10.192.208.250

loadaddr=0x82000000

netmask=255.255.255.0

ramboot=dhcp 82000000 $bootfile;dhcp 8f000000 $fdtfile;dhcp 88000000 $ramdiskfile;bootm 82000000 88000000 8f000000

ramdiskfile=ls1021atwr/fsl-image-x11-ls1021atwr.ext2.gz.u-boot

scsidevs=0

sdboot=fatload mmc 0 81000000 uImage; fatload mmc 0 8f000000 ls1021a-twr.dtb; fatload mmc 0 88000000 rootfs; bootm 81000000 88000000 8f000000

serverip=10.192.208.141

stderr=serial

stdin=serial

stdout=serial

usbboot=setenv bootargs root=/dev/sda1 rw console=$consoledev,$baudrate rootdelay=10;bootm 0x60120000 - 0x60020000

0 件の賞賛
返信