LS1012A Ethernet Queue status issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1012A Ethernet Queue status issue

跳至解决方案
1,266 次查看
Gyosun
Contributor III

Hello,

LSDK18.12 is being ported and applied to the LS1012A board.

There seems to be an issue where the LS1012A CPU utilization increases when sending Ethernet UDP packets, and this increase appears to be influenced by the performance of the receiving PC.

So, when transmitting UDP packets, it is necessary to check how much is accumulated in the QUEUE buffer.

I continued sending packets and checked the QUEUE status using the netstat -uan command, but it did not increase.

Please advise if there is a way to check the UDP QUEUE status other than netstat.

Thank you.

Best Regards,

Gyosun.

0 项奖励
回复
1 解答
1,207 次查看
LFGP
NXP TechSupport
NXP TechSupport

Hello Gyosun,

Please use the newest LSDK 21.08 due the driver for ethernet.

You can use SS instead NetStat

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,208 次查看
LFGP
NXP TechSupport
NXP TechSupport

Hello Gyosun,

Please use the newest LSDK 21.08 due the driver for ethernet.

You can use SS instead NetStat

 

0 项奖励
回复
1,151 次查看
Gyosun
Contributor III

Hi LFGP,

I'll give it a try.

Thank you for your help.

Best Regards.

Gyosun.

0 项奖励
回复