LLDP 5.15.71 add application issue based on LX2160ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLDP 5.15.71 add application issue based on LX2160ARDB

112 Views
jackho
Contributor IV

Hi,

We are trying to add docker-ce into yocto LLDP 5.15-71, but it shows below error:

Do you have any solution about ubuntu and yocto package conflicts issue?

bitbake ls-image-main

Error:
Problem: package util-linux-2.37.4-r0.aarch64 requires util-linux-libuuid, but none of the providers can be installed
- package ubuntu-main-22.04.1-r0.aarch64 conflicts with libuuid1 provided by libuuid1-2.37.4-r0.aarch64
- package ubuntu-main-22.04.1-r0.aarch64 obsoletes libuuid1 provided by libuuid1-2.37.4-r0.aarch64
- package docker-ce-20.10.12+ce+git906f57ff5b7100013dfef066ea8fe367706468df-r0.aarch64 requires util-linux, but none of the providers can be installed
- conflicting requests
(try to add '--allowerasing' to command line to replace conflicting packages or '--skip-broken' to skip uninstallable packages)

BR,

Jack Ho

Labels (1)
0 Kudos
Reply
1 Reply

64 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please unzip the attached file and put this recipe in sources/poky/meta/recipes-core/util-linux/util-linux-libuuid_2.38.1.bb

0 Kudos
Reply