U-Boot 2018.09-dirty (Oct 06 2020 - 11:34:29 +0000) SoC: LS1012AE Rev2.0 (0x87040020) Clock Configuration: CPU0(A53):1000 MHz Bus: 250 MHz DDR: 1000 MT/s Reset Configuration Word (RCW): 00000000: 0800000a 00000000 00000000 00000000 00000010: 33050000 c000000c 40000000 00001800 00000020: 00000000 00000000 00000000 000c4572 00000030: 00000000 1082a120 00000096 00000000 I2C: ready DRAM: 958 MiB WARNING: Calling __hwconfig without a buffer and before environment is ready Using SERDES1 Protocol: 13061 (0x3305) MMC: FSL_SDHC: 0, FSL_SDHC: 1 Loading Environment from SPI Flash... SF: Detected mx25u25645g with page size 256 Bytes, erase size 64 KiB, total 32 MiB SF: Warning - Only lower 16MiB accessible, Full access #define CONFIG_SPI_FLASH_BAR OK In: serial Out: serial Err: serial Model: FRWY-LS1012A Board Board: FRWY-LS1012A Version: unknownNet: PFE class pe firmware PFE tmu pe firmware eth0: pfe_eth0, eth1: pfe_eth1 Hit any key to stop autoboot: 0 => => => => => setenv mmc_boot 'pfe stop; if mmc dev ${devnum}; then setenv devtype mmc; run scan_dev_for_boot_part; fi' => setenv bootargs 'console=ttyS0,115200 root=/dev/mmcblk0p3 rw earlycon=uart8250,mmio,0x21c0500 rootdelay=3' => setenv bootcmd 'run distro_bootcmd; run sd_bootcmd; env exists secureboot && esbc_halt;' => saveenv Saving Environment to SPI Flash... SF: Detected mx25u25645g with page size 256 Bytes, erase size 64 KiB, total 32 MiB SF: Warning - Only lower 16MiB accessible, Full access #define CONFIG_SPI_FLASH_BAR Erasing SPI flash...Writing to SPI flash...done OK => boot Stopping PFE... switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... Scanning mmc 0:2... Found U-Boot script /ls1012afrwy_boot.scr 964 bytes read in 5 ms (187.5 KiB/s) ## Executing script at 80000000 17504768 bytes read in 892 ms (18.7 MiB/s) 14295 bytes read in 9 ms (1.5 MiB/s) ## Flattened Device Tree blob at 90000000 Booting using the fdt blob at 0x90000000 Using Device Tree in place at 0000000090000000, end 00000000900067d6 WARNING: fdt_fixup_stdout: could not read serial0 alias: FDT_ERR_NOTFOUND NOTICE: RNG: INSTANTIATED PCIe0: pcie@3400000 Root Complex: no link Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.9.140-dirty (root@fbubuntu) (gcc version 7.5.0 (Ubuntu/Linaro 7.5.0-3ubuntu1~18.04) ) #1 SMP PREEMPT Tue Oct 6 11:29:58 UTC 2020 [ 0.000000] Boot CPU: AArch64 Processor [410fd034] [ 0.000000] earlycon: uart8250 at MMIO 0x00000000021c0500 (options '') [ 0.000000] bootconsole [uart8250] enabled [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 16 MiB at 0x00000000bac00000 [ 0.000000] NUMA: No NUMA configuration found [ 0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000000bbdfffff] [ 0.000000] NUMA: Adding memblock [0x80000000 - 0xbbdfffff] on node 0 [ 0.000000] NUMA: Initmem setup node 0 [mem 0x80000000-0xbbdfffff] [ 0.000000] NUMA: NODE_DATA [mem 0xbbdde800-0xbbddffbf] [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000bbdfffff] [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x00000000bbdfffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bbdfffff] [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] psci: SMC Calling Convention v1.1 [ 0.000000] percpu: Embedded 22 pages/cpu @ffff80003bdc3000 s50904 r8192 d31016 u90112 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: enabling workaround for ARM erratum 845719 [ 0.000000] Built 1 zonelists in Node order, mobility grouping on. Total pages: 241416 [ 0.000000] Policy zone: DMA [ 0.000000] Kernel command line: console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500 root=PARTUUID=000068a6-03 rw rootwait [ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes) [ 0.000000] Memory: 917620K/980992K available (10876K kernel code, 966K rwdata, 4144K rodata, 1088K init, 916K bss, 46988K reserved, 16384K cma-reserved) [ 0.000000] Virtual kernel memory layout: [ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB) [ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB) [ 0.000000] .text : 0xffff000008080000 - 0xffff000008b20000 ( 10880 KB) [ 0.000000] .rodata : 0xffff000008b20000 - 0xffff000008f30000 ( 4160 KB) [ 0.000000] .init : 0xffff000008f30000 - 0xffff000009040000 ( 1088 KB) [ 0.000000] .data : 0xffff000009040000 - 0xffff000009131a00 ( 967 KB) [ 0.000000] .bss : 0xffff000009131a00 - 0xffff000009216dbc ( 917 KB) [ 0.000000] fixed : 0xffff7dfffe7fb000 - 0xffff7dfffec00000 ( 4116 KB) [ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB) [ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum) [ 0.000000] 0xffff7e0000000000 - 0xffff7e0000ef8000 ( 14 MB actual) [ 0.000000] memory : 0xffff800000000000 - 0xffff80003be00000 ( 958 MB) [ 0.000000] Preemptible hierarchical RCU implementation. [ 0.000000] Build-time adjustment of leaf fanout to 64. [ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=1. [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=1 [ 0.000000] NR_IRQS:64 nr_irqs:64 0 [ 0.000000] GIC: Using split EOI/Deactivate mode [ 0.000000] arm_arch_timer: Architected cp15 timer(s) running at 25.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns [ 0.000004] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns [ 0.008508] Console: colour dummy device 80x25 [ 0.013042] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000) [ 0.023486] pid_max: default: 32768 minimum: 301 [ 0.028225] Security Framework initialized [ 0.032602] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes) [ 0.040710] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes) [ 0.048054] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes) [ 0.054823] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes) [ 0.062913] ASID allocator initialised with 32768 entries [ 0.100969] EFI services will not be available. [ 0.121589] Brought up 1 CPUs [ 0.124576] SMP: Total of 1 processors activated. [ 0.129330] CPU features: detected feature: 32-bit EL0 Support [ 0.135213] CPU features: detected feature: Kernel page table isolation (KPTI) [ 0.145735] CPU: All CPU(s) started at EL2 [ 0.149873] alternatives: patching kernel code [ 0.155233] devtmpfs: initialized [ 0.162740] DMI not present or invalid. [ 0.166943] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.176812] futex hash table entries: 256 (order: 2, 16384 bytes) [ 0.183578] xor: measuring software checksum speed [ 0.228530] 8regs : 1919.000 MB/sec [ 0.272796] 8regs_prefetch: 1710.000 MB/sec [ 0.317410] 32regs : 2359.000 MB/sec [ 0.361665] 32regs_prefetch: 1982.000 MB/sec [ 0.366319] xor: using function: 32regs (2359.000 MB/sec) [ 0.371766] pinctrl core: initialized pinctrl subsystem [ 0.378875] NET: Registered protocol family 16 [ 0.395691] cpuidle: using governor menu [ 0.400204] vdso: 2 pages (1 code @ ffff000008b27000, 1 data @ ffff000009045000) [ 0.407820] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.415392] DMA: preallocated 256 KiB pool for atomic allocations [ 0.422162] Serial: AMBA PL011 UART driver [ 0.470987] HugeTLB registered 2 MB page size, pre-allocated 0 pages [ 0.561650] raid6: int64x1 gen() 394 MB/s [ 0.634114] raid6: int64x1 xor() 371 MB/s [ 0.706571] raid6: int64x2 gen() 598 MB/s [ 0.778982] raid6: int64x2 xor() 509 MB/s [ 0.851397] raid6: int64x4 gen() 903 MB/s [ 0.923782] raid6: int64x4 xor() 645 MB/s [ 0.996238] raid6: int64x8 gen() 836 MB/s [ 1.068641] raid6: int64x8 xor() 631 MB/s [ 1.141056] raid6: neonx1 gen() 623 MB/s [ 1.213468] raid6: neonx1 xor() 619 MB/s [ 1.285884] raid6: neonx2 gen() 1025 MB/s [ 1.358300] raid6: neonx2 xor() 879 MB/s [ 1.430723] raid6: neonx4 gen() 1323 MB/s [ 1.503123] raid6: neonx4 xor() 1007 MB/s [ 1.575532] raid6: neonx8 gen() 1433 MB/s [ 1.647944] raid6: neonx8 xor() 1051 MB/s [ 1.652249] raid6: using algorithm neonx8 gen() 1433 MB/s [ 1.657693] raid6: .... xor() 1051 MB/s, rmw enabled [ 1.662697] raid6: using intx1 recovery algorithm [ 1.673704] RCPM: layerscape_rcpm_init: The RCPM driver initialized. [ 1.682359] i2c i2c-0: IMX I2C adapter registered [ 1.688087] i2c i2c-0: can't use DMA, using PIO instead. [ 1.694128] pps_core: LinuxPPS API ver. 1 registered [ 1.699474] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 1.708828] PTP clock support registered [ 1.713194] dmi: Firmware registration failed. [ 1.718018] No BMan portals available! [ 1.722237] QMan: Allocated lookup table at ffff000009451000, entry count 65537 [ 1.729754] No QMan portals available! [ 1.733761] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree [ 1.741446] clocksource: Switched to clocksource arch_sys_counter [ 1.747937] VFS: Disk quotas dquot_6.6.0 [ 1.751977] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 1.774592] NET: Registered protocol family 2 [ 1.780115] TCP established hash table entries: 8192 (order: 4, 65536 bytes) [ 1.787450] TCP bind hash table entries: 8192 (order: 5, 131072 bytes) [ 1.794252] TCP: Hash tables configured (established 8192 bind 8192) [ 1.800796] UDP hash table entries: 512 (order: 2, 16384 bytes) [ 1.806816] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes) [ 1.813454] NET: Registered protocol family 1 [ 1.826188] RPC: Registered named UNIX socket transport module. [ 1.832187] RPC: Registered udp transport module. [ 1.836932] RPC: Registered tcp transport module. [ 1.841674] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 1.848636] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available [ 1.858633] audit: initializing netlink subsys (disabled) [ 1.864806] audit: type=2000 audit(1.752:1): initialized [ 1.875257] workingset: timestamp_bits=44 max_order=18 bucket_order=0 [ 1.882380] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 1.892522] NFS: Registering the id_resolver key type [ 1.897650] Key type id_resolver registered [ 1.901870] Key type id_legacy registered [ 1.905921] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 1.912948] fuse init (API version 7.26) [ 1.917218] SGI XFS with ACLs, security attributes, realtime, no debug enabled [ 1.937106] 9p: Installing v9fs 9p2000 file system support [ 1.942731] ceph: loaded (mds proto 32) [ 1.949386] async_tx: api initialized (async) [ 1.954034] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 1.965704] io scheduler noop registered [ 1.969762] io scheduler cfq registered (default) [ 1.976004] libphy: mdio_driver_register: phy-bcm-ns2-pci [ 1.983874] pci_hotplug: PCI Hot Plug PCI Core version: 0.5 [ 1.990457] pciehp: PCI Express Hot Plug Controller Driver version: 0.4 [ 1.998121] OF: PCI: host bridge /soc/pcie@3400000 ranges: [ 2.003904] OF: PCI: IO 0x4000010000..0x400001ffff -> 0x00000000 [ 2.010297] OF: PCI: MEM 0x4040000000..0x407fffffff -> 0x40000000 [ 2.016976] layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00 [ 2.023826] pci_bus 0000:00: root bus resource [bus 00-ff] [ 2.029379] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] [ 2.035631] pci_bus 0000:00: root bus resource [mem 0x4040000000-0x407fffffff] (bus address [0x40000000-0x7fffffff]) [ 2.046795] pci 0000:00:00.0: BAR 6: assigned [mem 0x4040000000-0x40400007ff pref] [ 2.054562] pci 0000:00:00.0: PCI bridge to [bus 01-ff] [ 2.060209] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt [ 2.071368] Freescale LS2 console driver [ 2.076748] fsl-ls2-console: device fsl_mc_console registered [ 2.082840] fsl-ls2-console: device fsl_aiop_console registered [ 2.090261] xenfs: not registering filesystem on non-xen platform [ 2.103763] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 2.112949] console [ttyS0] disabled [ 2.117324] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 15, base_baud = 7812500) is a 16550A [ 2.126287] console [ttyS0] enabled [ 2.126287] console [ttyS0] enabled [ 2.133380] bootconsole [uart8250] disabled [ 2.133380] bootconsole [uart8250] disabled [ 2.142444] SuperH (H)SCI(F) driver initialized [ 2.147631] msm_serial: driver initialized [ 2.152769] Unable to detect cache hierarchy for CPU 0 [ 2.235262] brd: module loaded [ 2.277575] loop: module loaded [ 2.283761] libphy: Fixed MDIO Bus: probed [ 2.290556] tun: Universal TUN/TAP device driver, 1.6 [ 2.296886] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com> [ 2.304277] Freescale FM module, FMD API version 21.1.0 [ 2.310342] Freescale FM Ports module [ 2.314111] fsl_mac: fsl_mac: FSL FMan MAC API based driver [ 2.319976] fsl_dpa: FSL DPAA Ethernet driver [ 2.324557] fsl_advanced: FSL DPAA Advanced drivers: [ 2.329601] fsl_proxy: FSL DPAA Proxy initialization driver [ 2.335333] fsl_oh: FSL FMan Offline Parsing port driver [ 2.341160] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI [ 2.348425] e1000: Copyright (c) 1999-2006 Intel Corporation. [ 2.354349] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k [ 2.360263] e1000e: Copyright(c) 1999 - 2015 Intel Corporation. [ 2.366348] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.4.0-k [ 2.373382] igb: Copyright (c) 2007-2014 Intel Corporation. [ 2.379079] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k [ 2.386981] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 2.393032] sky2: driver version 1.30 [ 2.398331] VFIO - User Level meta-driver version: 0.3 [ 2.409114] i2c /dev entries driver [ 2.417290] imx2-wdt 2ad0000.wdog: timeout 60 sec (nowayout=0) [ 2.425241] qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver [ 2.432822] sdhci: Secure Digital Host Controller Interface driver [ 2.439416] sdhci: Copyright(c) Pierre Ossman [ 2.444154] Synopsys Designware Multimedia Card Interface Driver [ 2.450927] sdhci-pltfm: SDHCI platform and OF driver helper [ 2.457399] [k] sdhci_add_host,3668, 1560000.esdhc [ 2.501468] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit [ 2.509572] [k] sdhci_add_host,3668, 1580000.esdhc [ 2.561461] mmc1: SDHCI controller on 1580000.esdhc [1580000.esdhc] using ADMA 64-bit [ 2.573646] caam-dma 1700000.crypto:caam-dma: Defer probing after JR driver probing [ 2.604246] caam 1700000.crypto: Instantiated RNG4 SH1 [ 2.611469] caam 1700000.crypto: device ID = 0x0a14040000000000 (Era [ 2.620277] caam 1700000.crypto: job rings = 3, qi = 0 [ 2.636855] caam algorithms registered in /proc/crypto [ 2.647440] caam_jr 1710000.jr: registering rng-caam [ 2.652611] caam 1700000.crypto: caam pkc algorithms registered in /proc/crypto [ 2.661571] DPAA2-ETH: debugfs created [ 2.667009] No fsl,qman node [ 2.670499] Freescale USDPAA process driver [ 2.674775] fsl-usdpaa: no region found [ 2.678824] Freescale USDPAA process IRQ driver [ 2.687352] optee: probing for conduit method from DT. [ 2.692769] mmc0: new high speed SDHC card at address 59b4 [ 2.699127] optee: api uid mismatch [ 2.702797] mmcblk0: mmc0:59b4 USDU1 7.51 GiB [ 2.708078] mmcblk0: p1 p2 p3 [ 2.718800] Netfilter messages via NETLINK v0.30. [ 2.726736] nf_conntrack version 0.5.0 (7680 buckets, 30720 max) [ 2.735001] nf_tables: (c) 2007-2009 Patrick McHardy <kaber@trash.net> [ 2.741582] nf_tables_compat: (c) 2012 Pablo Neira Ayuso <pablo@netfilter.org> [ 2.748855] mmc1: new HS200 MMC card at address 0001 [ 2.754546] ip_tables: (C) 2000-2006 Netfilter Core Team [ 2.760162] Initializing XFRM netlink socket [ 2.764482] mmcblk1: mmc1:0001 R1J55A 7.28 GiB [ 2.769412] NET: Registered protocol family 10 [ 2.773906] mmcblk1boot0: mmc1:0001 R1J55A partition 1 8.00 MiB [ 2.780433] mmcblk1boot1: mmc1:0001 R1J55A partition 2 8.00 MiB [ 2.790670] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 2.796833] mmcblk1rpmb: mmc1:0001 R1J55A partition 3 4.00 MiB [ 2.803500] mmcblk1: p1 [ 2.809221] NET: Registered protocol family 17 [ 2.813892] NET: Registered protocol family 15 [ 2.818416] Bridge firewalling registered [ 2.822527] Ebtables v2.0 registered [ 2.826233] 8021q: 802.1Q VLAN Support v1.8 [ 2.830480] 9pnet: Installing 9P2000 support [ 2.834908] Key type dns_resolver registered [ 2.839282] Key type ceph registered [ 2.847028] libceph: loaded (mon/osd proto 15/24) [ 2.852587] registered taskstats version 1 [ 2.861729] Btrfs loaded, crc32c=crc32c-generic [ 2.867812] caam-dma 1700000.crypto:caam-dma: caam dma support with 3 job rings [ 2.875580] hctosys: unable to open rtc device (rtc0) [ 2.882135] EXT4-fs (mmcblk0p3): couldn't mount as ext3 due to feature incompatibilities [ 3.119229] random: fast init done [ 3.344088] EXT4-fs (mmcblk0p3): recovery complete [ 3.351416] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null) [ 3.359577] VFS: Mounted root (ext4 filesystem) on device 179:3. [ 3.365704] devtmpfs: mounted [ 3.369463] Freeing unused kernel memory: 1088K [ 3.519841] EXT4-fs (mmcblk0p3): re-mounted. Opts: (null) Starting logging: OK Populating /dev using udev: [ 4.079106] udevd[1114]: starting version 3.2.5 [ 4.089292] random: udevd: uninitialized urandom read (16 bytes read) [ 4.096124] random: udevd: uninitialized urandom read (16 bytes read) [ 4.102903] random: udevd: uninitialized urandom read (16 bytes read) [ 4.120726] udevd[1114]: specified group 'input' unknown [ 4.145047] udevd[1115]: starting eudev-3.2.5 [ 4.577634] pfe: module is from the staging directory, the quality is unknown, you have been warned. [ 4.620274] cbus_baseaddr: ffff00000a000000, ddr_baseaddr: ffff800003400000, ddr_phys_baseaddr: 83400000, ddr_size: c00000 [ 4.677592] pfe_hw_init [ 4.680045] CLASS version: 20 [ 4.695715] TMU version: 1011231 [ 4.699295] BMU1 version: 21 [ 4.702317] BMU2 version: 21 [ 4.705198] EGPI1 version: 50 [ 4.708268] EGPI2 version: 50 [ 4.711304] HGPI version: 50 [ 4.714252] HIF version: 10 [ 4.717045] HIF NOPCY version: 10 [ 4.720457] bmu_init(1) done [ 4.723405] bmu_init(2) done [ 4.728575] class_init() done [ 4.741644] tmu_init() done [ 4.744439] gpi_init(1) done [ 4.747413] gpi_init(2) done [ 4.750364] gpi_init(hif) done [ 4.753417] bmu_enable(1) done [ 4.756565] bmu_enable(2) done [ 4.759688] pfe_hif_lib_init [ 4.762768] pfe_hif_init [ 4.765301] pfe_hif_alloc_descr [ 4.768729] pfe_hif_init_buffers [ 4.772840] pfe_firmware_init [ 4.780002] pfe_load_elf [ 4.782625] pe_load_ddr_section: load address(3fb0000) and elf file address(ffff0000095fb000) rcvd [ 4.814888] PFE binary version: pfe_ls1012a_slowpath_06 [ 4.820129] pfe_load_elf [ 4.823818] pfe_ctrl_init [ 4.826518] pfe_ctrl_init finished [ 4.829989] pfe_eth_init [ 4.832558] pfe_eth_mdio_init [ 4.847082] libphy: ls1012a MDIO Bus: probed [ 4.854625] pfe_phy_init interface 3 [ 4.858591] pfe 4000000.pfe eth0: pfe_eth_init_one: created interface, baseaddr: ffff00000a200000 [ 4.870768] pfe_phy_init interface 3 [ 4.874712] pfe 4000000.pfe eth1: pfe_eth_init_one: created interface, baseaddr: ffff00000a220000 [ 4.883901] pfe_debugfs_init done Initializing random number generator... done. Mounting cgroupfs hierarchy: OK Starting system message bus: [ 5.095283] urandom_read: 3 callbacks suppressed [ 5.095289] random: dbus-uuidgen: uninitialized urandom read (12 bytes read) [ 5.107152] random: dbus-uuidgen: uninitialized urandom read (8 bytes read) [ 5.132420] random: dbus-daemon: uninitialized urandom read (12 bytes read) dbus-daemon[1178]: Failed to start message bus: Could not get UID and GID for username "dbus" done Starting network: OK Starting dhcpcd... no interfaces ha[ 5.274929] pfe 4000000.pfe eth0: pfe_eth_open ve a carrier forked to background, child pid [ 5.282415] hif_process_client_req: register client_id 0 1207 [ 5.289038] pfe_hif_client_register [ 5.296298] pfe 4000000.pfe eth0: pfe_gemac_init [ 5.301937] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 5.309123] pfe 4000000.pfe eth1: pfe_eth_open [ 5.314395] hif_process_client_req: register client_id 1 [ 5.319763] pfe_hif_client_register [ 5.323895] pfe 4000000.pfe eth1: pfe_gemac_init ssh-keygen: generating new host keys: RSA [ 5.869471] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready [ 6.317936] pfe 4000000.pfe eth0: Link is Up - 1Gbps/Full - flow control rx/tx DSA ECDSA ED25519 Starting sshd: Privilege separation user sshd does not exist OK LSDK Buildroot LSDK login: root [root@LSDK ~]# ls rootfs_buildroot_arm64_moderate.tar [root@LSDK ~]# df -hT Filesystem Type Size Used Available Use% Mounted on /dev/root ext4 6.2G 255.3M 5.6G 4% / devtmpfs devtmpfs 448.1M 0 448.1M 0% /dev tmpfs tmpfs 456.6M 0 456.6M 0% /dev/shm tmpfs tmpfs 456.6M 44.0K 456.5M 0% /tmp tmpfs tmpfs 456.6M 100.0K 456.5M 0% /run cgroup tmpfs 456.6M 0 456.6M 0% /sys/fs/cgroup [root@LSDK ~]# uname -a Linux LSDK 4.9.140-dirty #1 SMP PREEMPT Tue Oct 6 11:29:58 UTC 2020 aarch64 GNU/Linux [root@LSDK ~]# rdate -s time.bora.net [root@LSDK ~]# tar xf rootfs_buildroot_arm64_moderate.tar [ 40.615952] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b [ 40.615952] [ 40.625115] CPU: 0 PID: 1 Comm: init Tainted: G C 4.9.140-dirty #1 [ 40.632433] Hardware name: LS1012A FRWY Board (DT) [ 40.637227] Call trace: [ 40.639682] [<ffff000008089570>] dump_backtrace+0x0/0x238 [ 40.645089] [<ffff0000080897bc>] show_stack+0x14/0x20 [ 40.650149] [<ffff0000084f1054>] dump_stack+0xa0/0xc4 [ 40.655209] [<ffff00000816064c>] panic+0x120/0x290 [ 40.660007] [<ffff0000080aafe8>] complete_and_exit+0x0/0x20 [ 40.665587] [<ffff0000080ab050>] do_group_exit+0x38/0xa0 [ 40.670907] [<ffff0000080b57d4>] get_signal+0xfc/0x4d0 [ 40.676052] [<ffff00000808871c>] do_signal+0x174/0x990 [ 40.681196] [<ffff0000080892a8>] do_notify_resume+0x88/0xa8 [ 40.686776] [<ffff000008083884>] work_pending+0x8/0x10 [ 40.691921] Kernel Offset: disabled [ 40.695409] Memory Limit: none [ 40.698466] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b [ 40.698466] |