Issues configuring DDR controller in Baremetal project.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues configuring DDR controller in Baremetal project.

ソリューションへジャンプ
1,765件の閲覧回数
rhaas
Contributor IV

I have been attempting to configure the DDR controller on a LS1028A dev board made by MYIR. This dev board is based on the NXP LS1028ARDB.

 

Since the end product is an avionics product, I cannot simply use uboot. I need to prune away code that may not be certifiable with the FAA.

 

Using uboot as a reference I have initialize the SMMU, TZPC, and CCI400. In addition, I keep the processor at EL3.

 

I have read the DDR controller registers using uboot. Using the QoriQ DDR configuration tool for the LS series, I imported those registers values. I have generated the bare metal C source code file,  InitDdrRegisters_1.c.

 

I seem to be able to write to the memory, but reading causes the processor to throw and exception.

 

I was wondering if anyone may have any idea of what might be missing in the initialization.

0 件の賞賛
返信
1 解決策
1,724件の閲覧回数
rhaas
Contributor IV

I just figured out my issue. It turns out that the NXP QorIQ DDR Tool, generates code for baremetal designs does an endian swap on the registers.

 

I didn’t feel this was odd because the old LS1021A processor that I used before required the endian swap. However the LS1028A processor’s DDR controller is little-endian.

Perhaps, the tool should be changed to not do the endian swap in the InitDdrRegisters_1.c file.

 

Ray Haas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,725件の閲覧回数
rhaas
Contributor IV

I just figured out my issue. It turns out that the NXP QorIQ DDR Tool, generates code for baremetal designs does an endian swap on the registers.

 

I didn’t feel this was odd because the old LS1021A processor that I used before required the endian swap. However the LS1028A processor’s DDR controller is little-endian.

Perhaps, the tool should be changed to not do the endian swap in the InitDdrRegisters_1.c file.

 

Ray Haas

0 件の賞賛
返信