Is there any way to write RCW, u-Boot into QSPI without an external rom writer?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there any way to write RCW, u-Boot into QSPI without an external rom writer?

跳至解决方案
1,607 次查看
Woon
Contributor III

in case of LS1012A board,

Is there any way to write RCW, u-Boot into QSPI without an external rom writer?

is it possible to write them into empty QSPI using JTAG?

or do I have to use external rom writer to write them into empty QSPI?

 

 

0 项奖励
回复
1 解答
1,562 次查看
williawh
Contributor III

I see. We are doing something similar. Our engineer developing the prototype is using a ls1046a chip and has procured CodeWarrior and CodeWarrior TAP to load/flash the blank chip if that helps or tells you anything.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,583 次查看
williawh
Contributor III

Woon,

The board you have is not from a Dev Kit from NXP? It is empty. Blank correct? You are not able to boot at power on correct?

0 项奖励
回复
1,579 次查看
Woon
Contributor III

the board is working well.

I just ask it for my custom board to development

 

 

0 项奖励
回复
1,563 次查看
williawh
Contributor III

I see. We are doing something similar. Our engineer developing the prototype is using a ls1046a chip and has procured CodeWarrior and CodeWarrior TAP to load/flash the blank chip if that helps or tells you anything.

0 项奖励
回复