in case of LS1012A board,
Is there any way to write RCW, u-Boot into QSPI without an external rom writer?
is it possible to write them into empty QSPI using JTAG?
or do I have to use external rom writer to write them into empty QSPI?
Solved! Go to Solution.
I see. We are doing something similar. Our engineer developing the prototype is using a ls1046a chip and has procured CodeWarrior and CodeWarrior TAP to load/flash the blank chip if that helps or tells you anything.
Woon,
The board you have is not from a Dev Kit from NXP? It is empty. Blank correct? You are not able to boot at power on correct?
the board is working well.
I just ask it for my custom board to development
I see. We are doing something similar. Our engineer developing the prototype is using a ls1046a chip and has procured CodeWarrior and CodeWarrior TAP to load/flash the blank chip if that helps or tells you anything.