Is there any way to write RCW, u-Boot into QSPI without an external rom writer?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any way to write RCW, u-Boot into QSPI without an external rom writer?

Jump to solution
1,864 Views
Woon
Contributor III

in case of LS1012A board,

Is there any way to write RCW, u-Boot into QSPI without an external rom writer?

is it possible to write them into empty QSPI using JTAG?

or do I have to use external rom writer to write them into empty QSPI?

 

 

0 Kudos
Reply
1 Solution
1,819 Views
williawh
Contributor III

I see. We are doing something similar. Our engineer developing the prototype is using a ls1046a chip and has procured CodeWarrior and CodeWarrior TAP to load/flash the blank chip if that helps or tells you anything.

View solution in original post

0 Kudos
Reply
3 Replies
1,840 Views
williawh
Contributor III

Woon,

The board you have is not from a Dev Kit from NXP? It is empty. Blank correct? You are not able to boot at power on correct?

0 Kudos
Reply
1,836 Views
Woon
Contributor III

the board is working well.

I just ask it for my custom board to development

 

 

0 Kudos
Reply
1,820 Views
williawh
Contributor III

I see. We are doing something similar. Our engineer developing the prototype is using a ls1046a chip and has procured CodeWarrior and CodeWarrior TAP to load/flash the blank chip if that helps or tells you anything.

0 Kudos
Reply