Hi,
I'm checking the User guide for LSSDK 19.09 and in the page 57 saiys:
• Check initial SNVS state
md 1e90014
88000900The second nibble indicates that the OTPMK is not blown
But if I execute the command, the output is like this:
=> md 1e90014
01e90014: 00000000 00000000 ........
Does it means my board has the secue boot fused?
Please provide as textual attachment complete U-Boot booting log and output of the "md 1e90BFC" command.
Hi,
I'm asking this because I've followed the guide to flash an image built with flex-builder and installed in a SD card with flex-installer and it doesn't boot.
I'm attaching three files:
- fullboot_error.txt -> This contains the whole boot until it fails trying to load the init
- uboot-md.txt -> Contains exactly what you asked for.
- uboot-printenv.txt -> Contains the output of printenv of u-boot
Let me know if you need anything else, thank you very much.
Was the board operational and capable to boot in factory-new state?
Yes, it's operational and can boot "TinyLSDK" boot, but not mine.
Please attach detailed description and logs corresponding to the image building with flex-builder and installation on SD card with flex-installer.