IFC_A16 and IFC_A17 pins of LS1020A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IFC_A16 and IFC_A17 pins of LS1020A

Jump to solution
824 Views
dainiuszilys
Contributor I

Hi there,

The datasheet of LS1020A says, that pins IFC_A16 - IFC_A20 can be pulled up or tristate (mark 5). Just a requirement - no pull-down.

The application note AN4878 says:

For LS1020A device configuration, IFC_A16 and IFC_A17 must be pulled up
during power-on reset.

Where is the truth? Can these pins be floating or not?

Labels (1)
Tags (1)
0 Kudos
1 Solution
725 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

These pins must be pulled up. As example see the IOT reference board schematics. The IFC_A16 is connected to 4.7k pull-up and to the chip select input of an external QSPI device. They refer to the mark 5 (Data sheet note 5).
LS102x_Note_5_pull_up.png

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
726 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

These pins must be pulled up. As example see the IOT reference board schematics. The IFC_A16 is connected to 4.7k pull-up and to the chip select input of an external QSPI device. They refer to the mark 5 (Data sheet note 5).
LS102x_Note_5_pull_up.png

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------