IDE alternative for LS1028ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IDE alternative for LS1028ARDB

1,055 Views
anesarkar
Contributor II

Is there any other IDE alternative for LS1028ARDB? 

And, do we need CodeWarrior Tap to build and run any program on the board?

0 Kudos
Reply
1 Reply

956 Views
alexander_yakov
NXP Employee
NXP Employee

For our Layerscape processors we offer CodeWarrior IDE integrated development software and CodeWarrior TAP debug probe.

CodeWarrior TAP is debug probe is used with CodeWarrior software, if you wish to use CodeWarrior debuger functionality. Debugger functionality is used to debug software, to flash onboard flash on "bare" board, and to bring up custom boards, designed based on LS1028ARDB reference schematic.

There are a number of third-party debug tool vendors. For more information about third-party tools please look the following discussion:

https://community.nxp.com/thread/500757

0 Kudos
Reply