How to resolve Synchronous Abort handler issue?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to resolve Synchronous Abort handler issue?

11,842 Views
naveennvn
Contributor III

Hi all,

I'm using LS2085AQDS Board with EAR5 images.

Default images only i flashed. Sometimes in uboot it throws synchronous abort handler error prints and hanging there itself. If i restart after sometime, its working fine.

Per day it throws 4 to 5 times. This is because my work is getting delay.

I want to know why this error is occured and how to resolve it ?. I tried to trace in uboot code. But i can't get exact reason of that.

If anyone know about this issue. Please help me on this. 

Boot log is as follows (error ptint is highlighted):

===========================================================================

U-Boot 2015.07-rc1Layerscape2-SDK+gfaa9145 (Dec 21 2015 - 15:34:49)

SoC:  LS2085E (0x87010010)

Clock Configuration:

       CPU0(A57):1600 MHz  CPU1(A57):1600 MHz  CPU2(A57):1600 MHz 

       CPU3(A57):1600 MHz  CPU4(A57):1600 MHz  CPU5(A57):1600 MHz 

       CPU6(A57):1600 MHz  CPU7(A57):1600 MHz 

       Bus:      600  MHz  DDR:      1333.333 MT/s     DP-DDR:   1333.333 MT/s

Reset Configuration Word (RCW):

       00: 40282830 40400040 00000000 00000000

       10: 00000000 00200000 00200000 00000000

       20: 0c212980 00002580 00000000 00000000

       30: 00000a08 00000000 00000080 00000080

       40: 00000000 00000000 00000000 00000000

       50: 00000000 00000000 00000000 00000000

       60: 00000000 00000000 00027000 00000000

       70: 3f350000 00000000 00000000 00000000

Model: Freescale Layerscape 2085a QDS Board

I2C:   ready

Board Arch: V1, Board Version: A

CPLD Version: A10

DRAM:  Initializing DDR....using SPD

Detected UDIMM 18ASF1G72HZ-2G1A1

Detected UDIMM 18ASF1G72HZ-2G1A1

15.5 GiB

DDR    15.5 GiB (DDR4, 64-bit, CL=9, ECC on)

       DDR Controller Interleaving Mode: 256B

       DDR Chip-Select Interleaving Mode: CS0+CS1

"Synchronous Abort" handler, esr 0x86000210

ELR:     fff21180

LR:      fff24858

x0 : 00000000fff92a00 x1 : 00000000fff929d0

x2 : 0000000000000040 x3 : 000000000000003f

x4 : 00000000fff8bb64 x5 : 000000004f790d52

x6 : 0000000000000000 x7 : 0000000000000000

x8 : 00000000ffffffff x9 : 00000000cff01000

x10: 0000000000000000 x11: 0000000000000000

x12: 0000000000000000 x13: 0000000000000000

x14: 0000000000000000 x15: 0000000000000000

x16: 0000000000000000 x17: 0000000000000002

x18: 00000000ffd1cd80 x19: 00000000fffb4f58

x20: 0000000000000000 x21: 00000000fff7f4ac

x22: 00000000fff90000 x23: 00000000fff8bc69

x24: 0000000000000001 x25: 0000000000000001

x26: 00000000fff90790 x27: 0000000000000000

x28: 00000000fff75738 x29: 000000003002008c

Resetting CPU ...

### ERROR ### Please RESET the board ###

===================================================================================

Thanks,

-Naveen

Labels (1)
2 Replies

7,418 Views
Pavel
NXP Employee
NXP Employee

Usually similar behavior happens if incorrect DDR setting is used on this board. Restart after sometime and since it happens throws 4 to 5 times, usually shows that some DDR setting is not fully correct for your board.

Try to test your board using different timing parameters for your board.

Test your DDR setting using Double Data Rate RAM Memory Validation (DDRV) or CodeWarrior Development Software for ARM v8 64-bit based QorIQ LS-Series Processors.

CodeWarrior Development Software for ARM v8 64-bit based QorIQ LS-Series Processors includes Double Data Rate RAM Memory Validation (DDRV).

Use the following pages:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7308947

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=6121481


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

7,418 Views
xiexn
Contributor I

Hi, I have the same issue.

My MCU is S32V234, and use two MT41K512M16HA-125 as the DDR.

What the configurations should be?

0 Kudos
Reply