Hello,
I am using ls1012afrdm board . After successfully updating u-boot on board using codewarrior TAP device did not come up again.
Case 1:
Steps Followed :
Case 2 :
After running above steps I tried to flash u-boot again using codewarrior studio but in between codewarrior studio stops.
Now when i am trying to connect device it gives me following error.
CCS: subcore error during multicore operation.
After running diagnostics i found following result.
Detail
Failed to execute target initialization script.
ERROR: Target reset failed.
Python Exception <class 'gdb.error'> Protocol error with Rcmd:
Traceback (most recent call last):
File "xxx/codewarrier/ProgrammerWorkspace/P2/.metadata/.plugins/com.freescale.debug.tcc/targetInit.py", line 298, in <module>
run_init_file()
File "xxx/codewarrier/ProgrammerWorkspace/P2/.metadata/.plugins/com.freescale.debug.tcc/targetInit.py", line 287, in run_init_file Reset()
File "xxx/codewarrier/ProgrammerWorkspace/P2/.metadata/.plugins/com.freescale.debug.tcc/targetInit.py", line 90, in Reset gdb.execute("py-reset %d" % user_reset_delay)
gdb.error: Error occurred in Python command: Protocol error with Rcmd
Failed to execute target initialization script
Please help me to fix this issue.
Help Appreciated.
Regards,
Kishan Patel
Original Attachment has been moved to: u-boot-qspi-2016.09+fslgit-r0.bin.zip
Solved! Go to Solution.
Hello Kishan Patel,
Probably RCW on QSPI flash has already been broken.
Please refer to the procedure described in the thread https://community.nxp.com/message/852508?commentID=852508#comment-852508 to do recovery.
Thanks,
Yiping
Hello Kishan Patel,
Probably RCW on QSPI flash has already been broken.
Please refer to the procedure described in the thread https://community.nxp.com/message/852508?commentID=852508#comment-852508 to do recovery.
Thanks,
Yiping
Hello yipingwang
I have bare board with LS1012ASE7HKA referenced from freedom. When I am trying to connect JTAG using codewarrior TAP at speed of 16000 it gives following error.
On freedom board i can connect code warrior with same configuration.
What could be the possible solution to flash image.
1) Does CMSIS debugger comes into picture for connecting Codewarrior to Processors JTAG?
I have flashed CMSIS Debugger bootloader and firmware and it is working ok.
2) Is there any changes on processor PLS1012ASE7HKA and LS1012ASE7HKA to connect with JTAG?
3) Do I need to modify LS1012A_FRDM_init.py for connecting JTAG with processor LS1012ASE7HKA?
Power up sequence , Clock(25MHz), and reset configuration match as per datasheet requirement.
Regards,
Kishan Patel