How to read Reset Request Status Register (BCFG_CCSR_RSTRQSR1)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to read Reset Request Status Register (BCFG_CCSR_RSTRQSR1)?

Jump to solution
2,014 Views
tracysmith
Contributor IV

After the kernel boots, seeing instability with frequent reboots on LS1043ARDB on idle. Need to check reset status register and see if this is a known issue on any QorIQ platform and what is the root cause if open defect or fixed.

How do we read the Reset Request Status Register (DCFG_CCSR_RSTRQSR1)?  Need the section of kernel code where reads should be done and an example needed. 

See section 12.3.14 Reset Request Status Register (DCFG_CCSR_RSTRQSR1) in chapter 12 Device Configuration and Pin Control. QorIQ LS1043A Reference Manual rev. 1 8/16. See LS1021A Reset Reason 

Labels (1)
Tags (1)
1 Solution
1,643 Views
tracysmith
Contributor IV

Codewarrior tap was connected to CPU Jtag with 10 pin gray cable. We measured with a scope, Tektronix TPS 2024. There was a short reset pulse estimated at about 10ms at TP6.  This is the same issue as DTCCS-148 and described below.

 

Lauterbach has good description of the ARM JTAG see:

http://www2.lauterbach.com/pdf/app_arm_jtag.pdf

also see note below on page 6:

 

“The debugger drives it open-drain. A 47 k pull-up is within the debug cable.

There might be the need to place a pull-up (1 k - 47 k) on target side to avoid

unintentional resets when the debugger is not connected and probably to strengthen

the weak 47 k pull-up in the debug cable”

Per the tools team this is a known issue:

 

see DTCCS-148

 

This was a problem with the CPLD on the LS1043ardb boards, it is fixed by updating the programming of the CPLD or a hardware rework. Boards replaced for CPLD update or hardware rework. Takes five days if replaced with already updated/reworked boards.

This can be closed as resolved.

View solution in original post

6 Replies
1,643 Views
tracysmith
Contributor IV

Not able to get the CPLD update instructions yet, but trying.  NXP wanting to exchange the boards takes 5 days.

0 Kudos
1,644 Views
tracysmith
Contributor IV

Codewarrior tap was connected to CPU Jtag with 10 pin gray cable. We measured with a scope, Tektronix TPS 2024. There was a short reset pulse estimated at about 10ms at TP6.  This is the same issue as DTCCS-148 and described below.

 

Lauterbach has good description of the ARM JTAG see:

http://www2.lauterbach.com/pdf/app_arm_jtag.pdf

also see note below on page 6:

 

“The debugger drives it open-drain. A 47 k pull-up is within the debug cable.

There might be the need to place a pull-up (1 k - 47 k) on target side to avoid

unintentional resets when the debugger is not connected and probably to strengthen

the weak 47 k pull-up in the debug cable”

Per the tools team this is a known issue:

 

see DTCCS-148

 

This was a problem with the CPLD on the LS1043ardb boards, it is fixed by updating the programming of the CPLD or a hardware rework. Boards replaced for CPLD update or hardware rework. Takes five days if replaced with already updated/reworked boards.

This can be closed as resolved.

1,643 Views
sinanakman
Senior Contributor III

Thanks Tracy for making this info available here, it will surely save lots of time in the future. The text mentions a CPLD fix, is this fix explained any where ?

Thanks and best regards

Sinan Akman

0 Kudos
1,643 Views
sinanakman
Senior Contributor III

Hi Tracy

You mentioned that the reset happens when CW TAP is configured. I assume your CW TAP is

connected to your board over JTAG at the time of the reboot. If this is the case, what is the debug state ? Are the resets/reboots happening during HALT ?

Regards

Sinan Akman

0 Kudos
1,643 Views
tracysmith
Contributor IV

On two separate LS1043A running SDK 2.0 1609, Codewarrior was not running at the time of the boots. Started CW4 initially on first power up merely to resume and CW was showing disconnected when checked, then reboots occur.

0 Kudos
1,643 Views
tracysmith
Contributor IV

This problem appears on SDK 2.0 1609 when Code Warrior TAP is configured. What is causing reboots?

0 Kudos