How to keep cache coherency between DPAA and Ctx-A53 on LS1043A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to keep cache coherency between DPAA and Ctx-A53 on LS1043A

跳至解决方案
2,459 次查看
uncoldice
Contributor II

Hi,

I am trying to use DPAA to transmit ethernet packet on LS1043ARDB board.

I use cache-enabled memory to encapsulate the ethernet packet data. When doing the qman portal enqueue operation, I have to flush the cache of this memory in order that DPAA can get proper data.

My question is: to avoid the load introduced by cache flush, is there an implement of the cache coherency between DPAA and ARM core in hardware? 

Thanks.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,118 次查看
bpe
NXP Employee
NXP Employee

FMAN DMA always issues snoopable transactions for buffers. If you are working with Linux SDK, make sure you did

not alter the kernel configuration to disable CCI-400 and SMMU support. If you are working in a non-Linux environment,

check Linux kernel source code, files arm-cci.c and arch/arm64/mm/dma-mapping.c (links below) for the corresponding attributes setting procedures:

http://git.freescale.com/git/cgit.cgi/ppc/sdk/linux.git/tree/drivers/bus/arm-cci.c?id=fsl-sdk-v2.0-1...
http://git.freescale.com/git/cgit.cgi/ppc/sdk/linux.git/tree/arch/arm64/mm/dma-mapping.c?id=fsl-sdk-...


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,119 次查看
bpe
NXP Employee
NXP Employee

FMAN DMA always issues snoopable transactions for buffers. If you are working with Linux SDK, make sure you did

not alter the kernel configuration to disable CCI-400 and SMMU support. If you are working in a non-Linux environment,

check Linux kernel source code, files arm-cci.c and arch/arm64/mm/dma-mapping.c (links below) for the corresponding attributes setting procedures:

http://git.freescale.com/git/cgit.cgi/ppc/sdk/linux.git/tree/drivers/bus/arm-cci.c?id=fsl-sdk-v2.0-1...
http://git.freescale.com/git/cgit.cgi/ppc/sdk/linux.git/tree/arch/arm64/mm/dma-mapping.c?id=fsl-sdk-...


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,118 次查看
uncoldice
Contributor II

Hi,

I have a new question about the CCI-400.

In LS1043ARM.pdf chapter 9.1.3, for the BMAN/QMAN/FMAN snoop transaction configuration, it says "Refer LS1043ADPAARM for more details". However, I cannot find any related information from LS1043ADPAARM Rev.0 04/2016.

Is there any updated DPAARM that contains this configuration? If yes, please share the way to get it.

Thank you.

0 项奖励
回复