How to do pin muxing on Freedom Ls1012A

cancel
Showing results for 
Search instead for 
Did you mean: 

How to do pin muxing on Freedom Ls1012A

697 Views
shyam_baldha
Contributor I

Hello Community,

Do we have only 'QorIQ Configuration and Validation Suite'  is the option to do pinmux on freedom LS1012A board ??

Can't we do the pin muxing as of its been done over all iMX platforms??

For Example: 

If I wants to configure a pin as GPIO which is configured as UART by default, The only thing I have to do on iMX platform is to change the muxing MACROs as below:  

from:     
pinctrl_uart1: uart1grp {            
fsl,pins = <    

     MX6QDL_PAD_SD3_DAT7__UART1_TX_DATA  0x1b0b1

     MX6QDL_PAD_SD3_DAT6__UART1_RX_DATA  0x1b0b1

               >;

        };

to:

      
pinctrl_uart1: uart1grp {

               
fsl,pins = <

       MX6QDL_PAD_SD3_DAT6__GPIO6_IO18        0x1b0b1

       MX6QDL_PAD_SD3_DAT7__GPIO6_IO17        0x1b0b1        
>;

        };

So is it possible to do the pinmuxing in a same way on FRDM-LS1012A  board?? If yes Please provide the proper documentation if not please Guide me on the other way to do pinmuxing on FRDM-LS1012A with proper documents.

Thanks,

Shyam

Labels (1)
0 Kudos
4 Replies

395 Views
ufedor
NXP TechSupport
NXP TechSupport

The LS1012A pin multiplexing is controlled by RCW fields and can't be altered during runtime - refer to the QorIQ LS1012A Reference Manual, 4.4.5.1 RCW Field Definitions.

You wrote:

> Do we have only 'QorIQ Configuration and Validation Suite'

> is the option to do pinmux on freedom LS1012A board ??

Yes, the QCVS PBL Tool can be used to create custom RCW.

0 Kudos

395 Views
2838219522
Contributor III

Is LS1021A also like this? Setting RCW is a only way to do pin muxing?

0 Kudos

395 Views
ufedor
NXP TechSupport
NXP TechSupport

Yes.

0 Kudos

395 Views
shyam_baldha
Contributor I

Thanks ufedor for your inputs.

0 Kudos