How to configure spi2 pins and uart2 pins on ls1021a twr board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure spi2 pins and uart2 pins on ls1021a twr board?

Jump to solution
681 Views
sujay1
Contributor V

I have a custom board based on ls1021a twr that has spi flash connected to spi2 and uart2 as a serial port

While trying to modify rcw configuration I found the following:

sujay1_0-1599039132005.png

and uart base as

 

sujay1_1-1599039192769.png

So If I configure uart_ext for spi2 then I won't be able to configure uart_base for uart_2, is there any way I can use spi2 and uart2?

0 Kudos
1 Solution
676 Views
Pavel
NXP Employee
NXP Employee

There is no possibility to use UART2 and SPI2. See the Table 3-3 in the LS1021a Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1021ARM

Use LPUART instead of UART2.

Have a great day,
Pavel Chubakov

View solution in original post

0 Kudos
1 Reply
677 Views
Pavel
NXP Employee
NXP Employee

There is no possibility to use UART2 and SPI2. See the Table 3-3 in the LS1021a Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1021ARM

Use LPUART instead of UART2.

Have a great day,
Pavel Chubakov

0 Kudos