How to configure an LX2160ARDB board for DPDK use with a DPL file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure an LX2160ARDB board for DPDK use with a DPL file

2,824 Views
Ncaseau
Contributor I

Hi,

I'm currently using DPDK applications on a LX2160ARDB board.The LSDK version the board is 21.08 and the MC firmware version is 10.28.1.

To configure the ports to be used with DPDK, I have followed the guidelines provided in the LSDK user guide : https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev21.08.pdf

For the moment I am able to configure the ports dynamically by using the dynamic_dpl.sh script.

I would now like to be able to freeze this configuration by using a DPL file. For that I generate a custom DPL file by using the restool generate-dpl command (after configuring the ports dynamically). Up to this point everything works fine.

I then try to flash the generated DPL file to the board following the instructions provided on your website : https://community.nxp.com/t5/Layerscape-Knowledge-Base/LX2160ARDB-How-to-update-MC-firmware-DPC-and-...

However, after resetting the board it seems that the modifications are not taken into account (ls-listni doesn't show the DPNIs configured to be used with DPDK) and when I reboot the board again the boot stops and I have to flash another DPL file in order for the board to work.

Could you help me? Is there something I'm doing wrong ?

Steps to reproduce :

- Use dynamic_dpl.sh scripts to configure the ports : ./dynamic_dpl.sh dpmac.3 dpmac.4

- Use restool generate-dpl command to generate a DPL file : restool dprc generate-dpl dprc.1 > dpl-file.dts

- Copy the .dts file to a Linux Host machine and run dtc tool to generate .dtb file : dtc -I dts -O dtb dpl-file.dts -o dpl-file.dtb

- Reboot the board and access U-boot command prompt

- Flash the .dtb file using a tftp server

- Reset the board

Nicolas

0 Kudos
Reply
4 Replies

2,194 Views
SERHIIHAVRYSH
Contributor I

Found the answer through parcing the dpaa2-eth driver from https://github.com/nxp-qoriq/linux with git tools:

/*

Date: Fri Oct 20 22:46:18 2023 +0300

dpaa2-mac: probe standalone DPMAC objects

In upstream, at the moment, we only support DPMAC objects which are
connected to DPNIs driver by the Linux kernel. To close the gap (aka
driver any other DPMAC object in TYPE_PHY) we build a standalone
driver around the dpaa2-mac.

Signed-off-by: Ioana Ciornei <ioana.ciornei@nxp.com>

*/

0 Kudos
Reply

2,227 Views
SERHIIHAVRYSH
Contributor I

I have the same issue, but my configuration is more complex with use of dpdmux instances.

Doing restool generate custom dpl.

Place it to mc_utils project.

Generate firmware*.img

And board stop boot when kernel initializes dpaa2 resources.

In generated dpl dpni for dpdk for example has next parameters

dpni@6 {
compatible = "fsl,dpni";
type = "DPNI_TYPE_NIC";
/* Unrecognized options found... */
options = "DPNI_OPT_HAS_KEY_MASKING";
num_queues = <16>;
num_tcs = <8>;
num_cgs = <24>;
mac_filter_entries = <16>;
vlan_filter_entries = <16>;
fs_entries = <1>;
qos_entries = <64>;
dist_key_size = <56>;
};

Comment inside looks like alarm...

0 Kudos
Reply

2,755 Views
June_Lu
NXP TechSupport
NXP TechSupport

Would you try LSDK21.08 4.1.13.6 Bringing up DPAA2 network interfaces

0 Kudos
Reply

2,744 Views
Ncaseau
Contributor I

Hello,

First of all thank you for your answer.

As you said, I tried bringing up the network interfaces (with ls-addni), generating a DPL file with the config and then flashing it to the board. It actually worked.

The problem might come from the dynamic_dpl script.

Nicolas

 

0 Kudos
Reply