How to check fm1-mac9 connection speed?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to check fm1-mac9 connection speed?

1,679 Views
gyosunshim
Contributor III

Hi NXP,

I am using LS1043A LSDK18.03-k4.9 custom board.

We are testing by connecting AQS-107 10G copper module to fm1-mac9.

Copper modules can be connected at various speeds as shown below.

aqs-107.png

The PC is 2.5G and connected to fm1-mac9.

When measuring iperf performance, it is estimated that it is connected to 2.5G with 1.2Gbps.

However, when I try ethtool fm1-mac9, the speed is not displayed as 2500Mb/s.

How can I check the connection speed on LS1043A?

Thank you for always helping,

Best regards.

gyosun.

Labels (1)
0 Kudos
Reply
3 Replies

1,606 Views
ufedor
NXP Employee
NXP Employee

Which SerDes protocol is in question?

Please consider that if MAC9 is configured as XFI, then only 10G physical data rate is supported.

0 Kudos
Reply

1,606 Views
gyosunshim
Contributor III

Hi ufedor,

MAC9 is connected by SerDes0 XFI.

SRDS_PRTCL_S1_RCW[128:143] = 0x1460.

Are you saying that if you connect like this, only 10G is supported, and it works according to the physical speed?

Is there any way to check what the connection speed is?

Or, is there a way to set the speed manually?

Thank you,

Best regards.

gyosun.

0 Kudos
Reply

1,606 Views
ufedor
NXP Employee
NXP Employee

> Is there any way to check what the connection speed is?

Request data from the PHY.

> Or, is there a way to set the speed manually?

This is not possible.

0 Kudos
Reply