How to check fm1-mac9 connection speed?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to check fm1-mac9 connection speed?

1,675件の閲覧回数
gyosunshim
Contributor III

Hi NXP,

I am using LS1043A LSDK18.03-k4.9 custom board.

We are testing by connecting AQS-107 10G copper module to fm1-mac9.

Copper modules can be connected at various speeds as shown below.

aqs-107.png

The PC is 2.5G and connected to fm1-mac9.

When measuring iperf performance, it is estimated that it is connected to 2.5G with 1.2Gbps.

However, when I try ethtool fm1-mac9, the speed is not displayed as 2500Mb/s.

How can I check the connection speed on LS1043A?

Thank you for always helping,

Best regards.

gyosun.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,602件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which SerDes protocol is in question?

Please consider that if MAC9 is configured as XFI, then only 10G physical data rate is supported.

0 件の賞賛
返信

1,602件の閲覧回数
gyosunshim
Contributor III

Hi ufedor,

MAC9 is connected by SerDes0 XFI.

SRDS_PRTCL_S1_RCW[128:143] = 0x1460.

Are you saying that if you connect like this, only 10G is supported, and it works according to the physical speed?

Is there any way to check what the connection speed is?

Or, is there a way to set the speed manually?

Thank you,

Best regards.

gyosun.

0 件の賞賛
返信

1,602件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is there any way to check what the connection speed is?

Request data from the PHY.

> Or, is there a way to set the speed manually?

This is not possible.

0 件の賞賛
返信