How can I restore NAND U-boot on LS1043A-RGW residential gateway?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I restore NAND U-boot on LS1043A-RGW residential gateway?

Jump to solution
1,912 Views
andrewbarrow
Contributor I

My U-boot is corrupted after I tried using a RDB U-boot image. I don't have Codewarrior TAP. After this happened I coulnd't boot, so I prepared an SD card with the RGW ASK (non-SD) U-boot image and two additional IRAM etc images as per instructions but that gets stuck and loops forever at the U-Boot version text.

Is there a specific SD card U-boot image for the RGW board? It is not provided as part of the pre-compiled ASK binaries for the RGW board.

I also tried the RDB u-boot (that's what corrupted my flash in the first place) and SD u-boot images, neither of which work.

Could you provide or point me to an SD card U-boot image for the LS1043A-RGW board or suggest a different recovery method?

Thanks!

Labels (1)
0 Kudos
Reply
1 Solution
1,685 Views
ufedor
NXP Employee
NXP Employee

Please try attached binary.

In case of further questions please create a Technical Case as described in:

https://community.nxp.com/thread/381898

View solution in original post

2 Replies
1,686 Views
ufedor
NXP Employee
NXP Employee

Please try attached binary.

In case of further questions please create a Technical Case as described in:

https://community.nxp.com/thread/381898

1,685 Views
andrewbarrow
Contributor I

This booted for me from SD... thanks kindly.

0 Kudos
Reply