How can I change the default serial of the u-boot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I change the default serial of the u-boot?

ソリューションへジャンプ
2,796件の閲覧回数
2838219522
Contributor III

I want change the default serial console in the u-boot,but I can't learn the source code of u-boot of ls1021atwr.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,471件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the Section 4.4.4.11 of NXP SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

Find the "LPUART console setting" in this Section.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,472件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the Section 4.4.4.11 of NXP SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

Find the "LPUART console setting" in this Section.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,471件の閲覧回数
2838219522
Contributor III

Thank you ,Pavel.

May I use other serials expect uart0 and lpuart0?

0 件の賞賛
返信