Hi Community,
I am working on LS1043ARDB development board and I am facing issues with secure boot.
I have performed following procedure for building secure boot sd card image,
Before performing all steps, I have made one change in configs/build_lsdk_config file I have set CONFIG_FUSE_PROVISIONING=y
1) Using Prebuilt Images
2) Using Custom Build
After performing above steps, I have inserted sd card into LS1043ardb but board is not booting up for both the procedures. If I have used non-secure boot image(firmware_ls1043ardb_uboot_sdboot.img) in above method then board is booting-up fine.
I want to know the detail step wise procedure for secure boot with example.
Thank you!
已解决! 转到解答。
See the following document about secure boot, OTPMK and SRKH:
http://cache.freescale.com/files/training/doc/ftf/2014/FTF-NET-F0070.pdf
See also the Chapter 6 of LSDK 1909 User Guide:
https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev19.09.pdf
Draw attention on the Section 6.1.1.7.2.2.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
See the following document about secure boot, OTPMK and SRKH:
http://cache.freescale.com/files/training/doc/ftf/2014/FTF-NET-F0070.pdf
See also the Chapter 6 of LSDK 1909 User Guide:
https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev19.09.pdf
Draw attention on the Section 6.1.1.7.2.2.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------