How Third party soft run on lx2160a board ??
Now our Third party soft is running on x86 centos server, but we want to run Third party soft on lx2160a board.
so,
1. Third party soft must be rebuilted with aarch64-linux-gnu-gcc ??
2. Third party soft can be rebuilted at CentOS environment ?? not at ubuntu18.04
3. if Third party soft need to be rebuilted with aarch64-linux-gnu-gcc, which version ??? is gcc version 7.5.0 ??
4 if we need to provide aarch64-linux-gnu-gcc source, LSDK have the GCC source ??? or where get the GCC source ???
5 if Third party soft is rebuilted at CentOS, the kenel of lx2160a board need to be centos ??? can use LSDK's default ubuntu18.04 kenel ???
Hi Yiping:
1 https://drive.google.com/open?id=1DKSXd775Beijes9eMguPfOroAxSWrF6G
this web address can not be open, I use 2 method, use foxconn's proxy, or use nomal net.
is this web address true ??
I am sorry,
1 in ubuntu18.04 and flexbuild_lsdk1909_update_311219.tgz envirment, I get that
zwb@ubuntu:~/lx2160a/flexbuild_lsdk1909_update_311219$ aarch64-linux-gnu-gcc-7 -v
Using built-in specs.
COLLECT_GCC=aarch64-linux-gnu-gcc-7
COLLECT_LTO_WRAPPER=/usr/lib/gcc-cross/aarch64-linux-gnu/7/lto-wrapper
Target: aarch64-linux-gnu
Configured with: ../src/configure -v --with-pkgversion='Ubuntu/Linaro 7.5.0-3ubuntu1~18.04' --with-bugurl=file:///usr/share/doc/gcc-7/README.Bugs --enable-languages=c,ada,c++,go,d,fortran,objc,obj-c++ --prefix=/usr --with-gcc-major-version-only --program-suffix=-7 --enable-shared --enable-linker-build-id --libexecdir=/usr/lib --without-included-gettext --enable-threads=posix --libdir=/usr/lib --enable-nls --with-sysroot=/ --enable-clocale=gnu --enable-libstdcxx-debug --enable-libstdcxx-time=yes --with-default-libstdcxx-abi=new --enable-gnu-unique-object --disable-libquadmath --disable-libquadmath-support --enable-plugin --enable-default-pie --with-system-zlib --enable-multiarch --enable-fix-cortex-a53-843419 --disable-werror --enable-checking=release --build=x86_64-linux-gnu --host=x86_64-linux-gnu --target=aarch64-linux-gnu --program-prefix=aarch64-linux-gnu- --includedir=/usr/aarch64-linux-gnu/include
Thread model: posix
gcc version 7.5.0 (Ubuntu/Linaro 7.5.0-3ubuntu1~18.04)
2 so , I use source to build and install aarch64-linux-gnu-gcc
https://releases.linaro.org/components/toolchain/gcc-linaro/latest-7/gcc-linaro-7.5-2019.12.tar.xz
but this code is accord with flexbuild_lsdk1909_update_311219.tgz 's aarch64-linux-gnu-gcc, ??
Dear Yiping:
when I use foxconn's proxy, I can access google, but the 3 website also can not be open,
use mobile's internet, without proxy, also can not access.
1 so, I go to Builds & Downloads - Linaro , and download aarch64-linux-gnu, https://releases.linaro.org/components/toolchain/binaries/latest-7/aarch64-linux-gnu/gcc-linaro-7.5....
is this cross-build tool true ?? is accord with my LSDK ?? I use this flexbuild_lsdk1909_update_311219.tgz
thanks
1. Third party software must be built with the ARM64 cross compiler aarch64-linux-gnu-gcc.
2. Third party soft can be rebuilt in CentOS environment.
3. Third party soft need to be rebuilt with any version cross compiler. LSDK 19.09 provides aarch64-linux-gnu-gcc version 7.5.
4. LSDK provides ARM64 cross compiler binary, LSDK installs aarch64-linux-gnu-gcc in /usr/bin/. However LSDK needs to be run in Ubuntu 18.04 or docker environment.
5. You can use LSDK default ubuntu18.04 rootfs.
Thanks,
Yiping
Dear Yiping:
1 if Third party soft will be rebuilt in CentOS, aarch64-linux-gnu-gcc compiler binary of LSDK can not be used。 I must supply the aarch64-linux-gnu-gcc source, third party soft can be rebuilt in CentOS environment.
2 where is aarch64-linux-gnu-gcc source ???? gcc v7.5.0 source of GCC web???
Thanks
You could download Yocto SDK from the following link.
readme - qoriq-components/yocto-sdk - Repo manifest for QorIQ Yocto SDK
Then build Toolchian with the following command.
$ source setup-env -m lx2160ardb
$ bitbake fsl-toolchain
Thanks,
Yiping
Dear Yiping:
for lx2160ardb board, we use the SDK is flexbuild_lsdk1909_update_311219.tgz , is not QorIQ Linux SDK v2.0,
so I find that toolchain of building is aarch64-linux-gnu-gcc .
1 do as below, can I built out aarch64-linux-gnu-gcc ??
You could download Yocto SDK from the following link.
readme - qoriq-components/yocto-sdk - Repo manifest for QorIQ Yocto SDK
Then build Toolchian with the following command.
$ source setup-env -m lx2160ardb
$ bitbake fsl-toolchain
2 or , get gcc v7.5.0 source of GCC web, can built out aarch64-linux-gnu-gcc ??
Thanks!
I uploaded GCC 9.2 Toolchain installation file for ARCH arm64 platforms, which is built from Yocto 3.0 release.
https://drive.google.com/open?id=1DKSXd775Beijes9eMguPfOroAxSWrF6G
Please install this Toolchain with the following procedure.
$ chmod 777 fsl-qoriq-glibc-x86_64-fsl-toolchain-aarch64-toolchain-3.0.sh
$./fsl-qoriq-glibc-x86_64-fsl-toolchain-aarch64-toolchain-3.0.sh
$ source environment-setup-aarch64-fsl-linux
$ aarch64-fsl-linux-gcc --version
Dear Yiping:
1 https://drive.google.com/open?id=1DKSXd775Beijes9eMguPfOroAxSWrF6G
fsl-qoriq-glibc-x86_64-fsl-toolchain-aarch64-toolchain-3.0.sh
$./fsl-qoriq-glibc-x86_64-fsl-toolchain-aarch64-toolchain-3.0.sh
the 3 web address all can not be open, I use 2 method, use foxconn's proxy, or use nomal net.
is web address true ??