HiLS1021A: Rev 2 : Can confirm the JTAG connector for Dstream is J12?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HiLS1021A: Rev 2 : Can confirm the JTAG connector for Dstream is J12?

ソリューションへジャンプ
1,686件の閲覧回数
shrikant_bobade
Contributor III

Hi,

I want to use Dstream DSTREAM – ARM Developer  for debugging along with LS1021A rev:2.0, I am using a 10 pin JTAG connector for connection at J12 connector. Is it correct connector ?

In Dstream case K20 JTAG  connector should not be used ?

Any pointers or references will be a great help!

Thanks

Shrikant

ラベル(1)
タグ(1)
1 解決策
1,538件の閲覧回数
ufedor
NXP Employee
NXP Employee

Is your request about the TWR-LS1021A board?

If "yes", then J12 has to be used for the debugger connection.

元の投稿で解決策を見る

4 返答(返信)
1,538件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which NXP board is in question?

Please note that we do not support third-party tools.

1,538件の閲覧回数
shrikant_bobade
Contributor III

Hi,

Board in question:  Layerscape 1021A rev 2.0: QorIQ LS1021A Dual-Core Communications Processor wi|NXP

Thanks for an update.

Thanks

Shrikant

0 件の賞賛
返信
1,539件の閲覧回数
ufedor
NXP Employee
NXP Employee

Is your request about the TWR-LS1021A board?

If "yes", then J12 has to be used for the debugger connection.

1,538件の閲覧回数
shrikant_bobade
Contributor III

yes, TWR-LS1021A board, Thanks for confirming the J12 JTAG connector.

Thanks

Shrikant

0 件の賞賛
返信