Fetch failed when to try real-time-edge v2.6 for ls1028;

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fetch failed when to try real-time-edge v2.6 for ls1028;

Jump to solution
1,854 Views
xinliwang
Contributor III

Hi @yipingwang 

I got an error when I try to bitbake nxp-image-real-time-edge v2.6 for ls1028 board;

xinliwang_0-1692153719766.png

for the url I try it on my browser and it pops 404 error like down below:

http://etherlab.org/download/ethercat/

xinliwang_1-1692153888846.png

it doesn't have this page?

Tags (1)
0 Kudos
Reply
1 Solution
1,550 Views
Irene
NXP Pro Support
NXP Pro Support

Hello,

  The tarball that you need can be found at:

www.nxp.com/lgfiles/updates/other/ethercat-1.5.2.tar.bz2

 

Regards,

Irene

View solution in original post

0 Kudos
Reply
8 Replies
1,551 Views
Irene
NXP Pro Support
NXP Pro Support

Hello,

  The tarball that you need can be found at:

www.nxp.com/lgfiles/updates/other/ethercat-1.5.2.tar.bz2

 

Regards,

Irene

0 Kudos
Reply
1,829 Views
Irene
NXP Pro Support
NXP Pro Support

Are you using the NXP release or something upstream?  are you following the steps outlined in the attached document which can be found on the nxp.com website.

0 Kudos
Reply
1,813 Views
xinliwang
Contributor III

Hi @Irene 

Yes, I just follow the step as reference menu told. 

Did you check the link I post? I think there is no way i can fetch if the link doesn't work.

0 Kudos
Reply
1,840 Views
Irene
NXP Pro Support
NXP Pro Support

Let me look into this issue.

0 Kudos
Reply
1,767 Views
xinliwang
Contributor III

Hi, @Irene 

Any ideas for my problem?

0 Kudos
Reply
1,703 Views
Irene
NXP Pro Support
NXP Pro Support

Which release are you used ? I dont find nxp-image-real-time-edge in our 6.1.22 release.

0 Kudos
Reply
1,638 Views
xinliwang
Contributor III

@Irene 

I'm not the only person who has the same issue. 

Please check the link https://github.com/nxp-real-time-edge-sw/yocto-real-time-edge/issues/7

xinliwang_0-1693190604408.png

 

0 Kudos
Reply
1,687 Views
xinliwang
Contributor III

Hi, @Irene

I don't get it what do you mean that you dont find nxp-image-real-time-edge”?

According to the reference menu RTEDGEYOCTOUG_Rev2.6 on page 8, Yocto Project build uses the bitbake command.

xinliwang_0-1692836451658.png

 

0 Kudos
Reply