Hi @yipingwang
I got an error when I try to bitbake nxp-image-real-time-edge v2.6 for ls1028 board;
for the url I try it on my browser and it pops 404 error like down below:
http://etherlab.org/download/ethercat/
it doesn't have this page?
Solved! Go to Solution.
Hello,
The tarball that you need can be found at:
www.nxp.com/lgfiles/updates/other/ethercat-1.5.2.tar.bz2
Regards,
Irene
View solution in original post
Are you using the NXP release or something upstream? are you following the steps outlined in the attached document which can be found on the nxp.com website.
Hi @Irene
Yes, I just follow the step as reference menu told.
Did you check the link I post? I think there is no way i can fetch if the link doesn't work.
Let me look into this issue.
Hi, @Irene
Any ideas for my problem?
Which release are you used ? I don’t find “nxp-image-real-time-edge” in our 6.1.22 release.
@Irene
I'm not the only person who has the same issue.
Please check the link https://github.com/nxp-real-time-edge-sw/yocto-real-time-edge/issues/7
I don't get it what do you mean that you don’t find “nxp-image-real-time-edge”?
According to the reference menu RTEDGEYOCTOUG_Rev2.6 on page 8, Yocto Project build uses the bitbake command.