Failed to get PTP Hardware Clock support on LA1224ARDB

cancel
Showing results for 
Search instead for 
Did you mean: 

Failed to get PTP Hardware Clock support on LA1224ARDB

Jump to solution
240 Views
NXP Employee
NXP Employee

Hi

I'd like to verify the PTP feature on LA1224ARDB. Tried the prebuild and rebuilt Linux kernels with PTP related options on. However, failed to get PTP Hardware Clock support on eth0/eth1 and there is no /dev/ptp and /dev/pps generated. Could you give me some hints? Thanks.

a.jpg

Here are related info:

Board: LA1224-RDB, Board version: A

BSP: 0.6

 

Kernel PTP related options loaded:

b.jpg

Device tree (fsl-lx2160a.dtsi) PTP related info:

c.jpg

Labels (1)
0 Kudos
1 Solution
179 Views
NXP Employee
NXP Employee

Thanks. I got it solved by updating the DPL file to enable PTP.

View solution in original post

0 Kudos
2 Replies
205 Views
NXP TechSupport
NXP TechSupport

Hello Tony Hsu,

Please check whether the following options are enable in your Kernel configuration file.

CONFIG_FSL_DPAA2_ETH

CONFIG_FSL_DPAA2_PTP_CLOCK

Thanks,

Yiping

0 Kudos
180 Views
NXP Employee
NXP Employee

Thanks. I got it solved by updating the DPL file to enable PTP.

View solution in original post

0 Kudos