Failed to get PTP Hardware Clock support on LA1224ARDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Failed to get PTP Hardware Clock support on LA1224ARDB

跳至解决方案
4,276 次查看
nxf47487
NXP Employee
NXP Employee

Hi

I'd like to verify the PTP feature on LA1224ARDB. Tried the prebuild and rebuilt Linux kernels with PTP related options on. However, failed to get PTP Hardware Clock support on eth0/eth1 and there is no /dev/ptp and /dev/pps generated. Could you give me some hints? Thanks.

a.jpg

Here are related info:

Board: LA1224-RDB, Board version: A

BSP: 0.6

 

Kernel PTP related options loaded:

b.jpg

Device tree (fsl-lx2160a.dtsi) PTP related info:

c.jpg

标签 (1)
0 项奖励
回复
1 解答
4,215 次查看
nxf47487
NXP Employee
NXP Employee

Thanks. I got it solved by updating the DPL file to enable PTP.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,241 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Tony Hsu,

Please check whether the following options are enable in your Kernel configuration file.

CONFIG_FSL_DPAA2_ETH

CONFIG_FSL_DPAA2_PTP_CLOCK

Thanks,

Yiping

0 项奖励
回复
4,216 次查看
nxf47487
NXP Employee
NXP Employee

Thanks. I got it solved by updating the DPL file to enable PTP.

0 项奖励
回复