Ethernet PHY for LS1043A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet PHY for LS1043A

2,785 次查看
carljones
Contributor III

Hello,

I would like to ask if the following PHYs will work with LS1043A as replacement for the RGMII and SGMII PHYs.

If not, what Ethernet PHYs could I use other than the ones specified in the RDB?

Thank you very much.

Best,

Carlos

标签 (1)
0 项奖励
回复
2 回复数

2,487 次查看
bpe
NXP Employee
NXP Employee

Please be aware, that we do not test third-party Ethernet PHYs
against our processors and do not keep an officially "approved" PHY
list. Instead, we emphasize on the compatibility of MAC/PHY interfaces
of our processors to the respective  standard specifications to
allows our customers to have the maximum wide choice of third-party
components. Our response to your inquiry therefore is, you can use
your PHY devices al long as they satisfy the requirements of the
supported interface between the MAC and the PHY and the requirements
of the processor Datasheet.

Regards,

Platon

2,487 次查看
carljones
Contributor III

Thank you, bpe.

Best,

Carlos

0 项奖励
回复