Errors building `fsl-image-virt` image for LS1046ARDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Errors building `fsl-image-virt` image for LS1046ARDB

跳至解决方案
1,794 次查看
mharshe
Contributor I

Hi

I'm trying to build the image with virtualization support for the LS 1046ARDB target on an Ubuntu 16.04 machine (aarch64). I've been running into various problems  - some of which I could solve by setting some compile tag flags.

For pkgconfig, I had to set the following cflags:

CFLAGS_class-native += " -Wno-error=format-nonliteral -Wno-error=unused-variable"
CFLAGS_class-nativesdk += " -Wno-error=format-nonliteral -Wno-error=unused-variable"

 

But now I'm getting errors for elfutils

ERROR: oe_runmake failed
ERROR: Function failed: do_compile (log file is located at /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/temp/log.do_compile.6577)
ERROR: Logfile of failure stored in: /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/temp/log.do_compile.6577
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 4
| make  all-recursive
| make[1]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/build'
| Making all in config
| make[2]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/build/config'
| make[2]: Nothing to be done for 'all'.
| make[2]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/build/config'
| Making all in m4
| make[2]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/build/m4'
| make[2]: Nothing to be done for 'all'.
| make[2]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/build/m4'
| Making all in lib
| make[2]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/build/lib'
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/../libelf -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror -fpic -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o xstrdup.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/xstrdup.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/../libelf -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror -fpic -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o xstrndup.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/xstrndup.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/../libelf -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144 -ffunction-sections -Werror -fpic -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o xmalloc.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/xmalloc.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/../libelf -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror -fpic -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o next_prime.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/next_prime.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/../libelf -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror -fpic -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o crc32.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/crc32.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/../libelf -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror -fpic -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o crc32_file.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/crc32_file.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/../libelf -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror -fpic -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o md5.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/md5.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/../libelf -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror -fpic -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o sha1.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/sha1.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/../libelf -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror -fpic -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o color.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/color.c
| rm -f libeu.a
| ar cru libeu.a xstrdup.o xstrndup.o xmalloc.o next_prime.o crc32.o crc32_file.o md5.o sha1.o color.o
| ranlib libeu.a
| make[2]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/build/lib'
| Making all in libelf
| make[2]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/build/libelf'
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf_version.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf_version.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf_hash.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf_hash.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf_error.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf_error.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf_fill.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf_fill.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf_begin.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf_begin.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf_next.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf_next.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf_rand.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf_rand.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf_end.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf_end.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf_kind.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf_kind.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o gelf_getclass.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/gelf_getclass.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf_getbase.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf_getbase.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf_getident.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf_getident.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf32_fsize.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf32_fsize.c
| gcc  -D_GNU_SOURCE -DHAVE_CONFIG_H -DLOCALEDIR='"/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/share/locale"' -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I..  -I. -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib -I.. -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -std=gnu99 -Wall -Wshadow -Werror -Wunused -Wextra -fgnu89-inline -Wformat=2 -Wstack-usage=262144  -Werror  -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -c -o elf64_fsize.o /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf64_fsize.c
| In file included from ../config.h:115,
|                  from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf32_fsize.c:31:
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/libelfP.h:50:30: error: '__elf32_msize' specifies less restrictive attribute than its target 'elf32_fsize': 'const' [-Werror=missing-attributes]
|    50 | #define __elfw2_(Bits, Name) __elf##Bits##_##Name
|       |                              ^~~~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/eu-config.h:60:26: note: in definition of macro 'strong_alias'
|    60 |   extern __typeof (name) aliasname __attribute__ ((alias (#name)));
|       |                          ^~~~~~~~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf32_fsize.c:71:1: note: in expansion of macro 'local_strong_alias'
|    71 | local_strong_alias (elfw2(LIBELFBITS, fsize), __elfw2(LIBELFBITS, msize))
|       | ^~~~~~~~~~~~~~~~~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/libelfP.h:55:29: note: in expansion of macro '__elfw2_'
|    55 | #define __elfw2(Bits, Name) __elfw2_(Bits, Name)
|       |                             ^~~~~~~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf32_fsize.c:71:47: note: in expansion of macro '__elfw2'
|    71 | local_strong_alias (elfw2(LIBELFBITS, fsize), __elfw2(LIBELFBITS, msize))
|       |                                               ^~~~~~~
| In file included from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf32_fsize.c:35:
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/libelfP.h:51:28: note: '__elf32_msize' target declared here
|    51 | #define elfw2_(Bits, Name) elf##Bits##_##Name
|       |                            ^~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/libelfP.h:56:27: note: in expansion of macro 'elfw2_'
|    56 | #define elfw2(Bits, Name) elfw2_(Bits, Name)
|       |                           ^~~~~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf32_fsize.c:43:1: note: in expansion of macro 'elfw2'
|    43 | elfw2(LIBELFBITS, fsize) (type, count, version)
|       | ^~~~~
| cc1: all warnings being treated as errors
| Makefile:685: recipe for target 'elf32_fsize.o' failed
| make[2]: *** [elf32_fsize.o] Error 1
| make[2]: *** Waiting for unfinished jobs....
| In file included from ../config.h:115,
|                  from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf32_fsize.c:31,
|                  from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf64_fsize.c:31:
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/libelfP.h:50:30: error: '__elf64_msize' specifies less restrictive attribute than its target 'elf64_fsize': 'const' [-Werror=missing-attributes]
|    50 | #define __elfw2_(Bits, Name) __elf##Bits##_##Name
|       |                              ^~~~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/lib/eu-config.h:60:26: note: in definition of macro 'strong_alias'
|    60 |   extern __typeof (name) aliasname __attribute__ ((alias (#name)));
|       |                          ^~~~~~~~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf32_fsize.c:71:1: note: in expansion of macro 'local_strong_alias'
|    71 | local_strong_alias (elfw2(LIBELFBITS, fsize), __elfw2(LIBELFBITS, msize))
|       | ^~~~~~~~~~~~~~~~~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/libelfP.h:55:29: note: in expansion of macro '__elfw2_'
|    55 | #define __elfw2(Bits, Name) __elfw2_(Bits, Name)
|       |                             ^~~~~~~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf32_fsize.c:71:47: note: in expansion of macro '__elfw2'
|    71 | local_strong_alias (elfw2(LIBELFBITS, fsize), __elfw2(LIBELFBITS, msize))
|       |                                               ^~~~~~~
| In file included from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf32_fsize.c:35,
|                  from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf64_fsize.c:31:
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/libelfP.h:51:28: note: '__elf64_msize' target declared here
|    51 | #define elfw2_(Bits, Name) elf##Bits##_##Name
|       |                            ^~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/libelfP.h:56:27: note: in expansion of macro 'elfw2_'
|    56 | #define elfw2(Bits, Name) elfw2_(Bits, Name)
|       |                           ^~~~~~
| /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/elfutils-0.163/libelf/elf32_fsize.c:43:1: note: in expansion of macro 'elfw2'
|    43 | elfw2(LIBELFBITS, fsize) (type, count, version)
|       | ^~~~~
| cc1: all warnings being treated as errors
| Makefile:685: recipe for target 'elf64_fsize.o' failed
| make[2]: *** [elf64_fsize.o] Error 1
| make[2]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/build/libelf'
| Makefile:475: recipe for target 'all-recursive' failed
| make[1]: *** [all-recursive] Error 1
| make[1]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/build'
| Makefile:391: recipe for target 'all' failed
| make: *** [all] Error 2
| WARNING: exit code 1 from a shell command.
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (log file is located at /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/elfutils-native/0.163-r0/temp/log.do_compile.6577)
ERROR: Task 480 (virtual:native:/home/ubuntu/development/thirdparties/nxp_yocto/sources/poky/meta/recipes-devtools/elfutils/elfutils_0.163.bb, do_compile) failed with exit code '1'

 

On another run I also got an error compiling gcc:

DEBUG: SITE files ['endian-little', 'bit-64', 'arm-common', 'arm-64', 'common-linux', 'common-glibc', 'aarch64-linux', 'common']
DEBUG: Executing shell function do_compile
NOTE: make -j 4 all-host configure-target-libgcc
make[1]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libiberty'
make[2]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libiberty/testsuite'
make[2]: Nothing to be done for 'all'.
make[2]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libiberty/testsuite'
make[1]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libiberty'
make[1]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/intl'
make[1]: Nothing to be done for 'all'.
make[1]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/intl'
make[1]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/build-aarch64-linux/libiberty'
make[1]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libbacktrace'
make  all-am
make[2]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/build-aarch64-linux/libiberty/testsuite'
make[2]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libbacktrace'
true  DO=all multi-do # make
make[2]: Nothing to be done for 'all'.
make[2]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/build-aarch64-linux/libiberty/testsuite'
make[2]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libbacktrace'
make[1]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libbacktrace'
make[1]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/build-aarch64-linux/libiberty'
make[1]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libdecnumber'
make[1]: Nothing to be done for 'all'.
make[1]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libdecnumber'
make[1]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/fixincludes'
make[1]: Nothing to be done for 'all'.
make[1]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/fixincludes'
make[1]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/lto-plugin'
make[1]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/build-aarch64-linux/fixincludes'
make[1]: Nothing to be done for 'all'.
make[1]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/build-aarch64-linux/fixincludes'
make  all-am
make[1]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libcpp'
test -f config.h || (rm -f stamp-h1 && make stamp-h1)
make[2]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/lto-plugin'
make[1]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/libcpp'
make[2]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/lto-plugin'
make[1]: Leaving directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/lto-plugin'
make[1]: Entering directory '/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work/aarch64-linux/gcc-cross-aarch64/linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/build.aarch64-linux.aarch64-fsl-linux/gcc'
g++    -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -DIN_GCC  -DCROSS_DIRECTORY_STRUCTURE  -fno-exceptions -fno-rtti -fasynchronous-unwind-tables -W -Wall -Wno-narrowing -Wwrite-strings -Wcast-qual -Wmissing-format-attribute -pedantic -Wno-long-long -Wno-variadic-macros -Wno-overlength-strings   -DHAVE_CONFIG_H -static-libstdc++ -static-libgcc -L/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/lib -L/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/lib -Wl,-rpath-link,/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/lib -Wl,-rpath-link,/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/lib -Wl,-rpath,/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/lib -Wl,-rpath,/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/lib -Wl,-O1 gcov.o libcommon.a ../libcpp/libcpp.a   ../libbacktrace/.libs/libbacktrace.a ../libiberty/libiberty.a ../libdecnumber/libdecnumber.a  -o gcov
g++    -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -DIN_GCC  -DCROSS_DIRECTORY_STRUCTURE  -fno-exceptions -fno-rtti -fasynchronous-unwind-tables -W -Wall -Wno-narrowing -Wwrite-strings -Wcast-qual -Wmissing-format-attribute -pedantic -Wno-long-long -Wno-variadic-macros -Wno-overlength-strings   -DHAVE_CONFIG_H -static-libstdc++ -static-libgcc -L/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/lib -L/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/lib -Wl,-rpath-link,/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/lib -Wl,-rpath-link,/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/lib -Wl,-rpath,/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/lib -Wl,-rpath,/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/lib -Wl,-O1 gcov-dump.o \
	libcommon.a ../libcpp/libcpp.a   ../libbacktrace/.libs/libbacktrace.a ../libiberty/libiberty.a ../libdecnumber/libdecnumber.a  -o gcov-dump
g++  -c  -DIN_GCC_FRONTEND -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -DIN_GCC  -DCROSS_DIRECTORY_STRUCTURE  -fno-exceptions -fno-rtti -fasynchronous-unwind-tables -W -Wall -Wno-narrowing -Wwrite-strings -Wcast-qual -Wmissing-format-attribute -pedantic -Wno-long-long -Wno-variadic-macros -Wno-overlength-strings   -DHAVE_CONFIG_H -I. -Icp -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../include -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libcpp/include -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include  -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libdecnumber -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libdecnumber/dpd -I../libdecnumber -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libbacktrace    -o cp/except.o -MT cp/except.o -MMD -MP -MF cp/.deps/except.TPo /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/except.c
g++  -c  -DIN_GCC_FRONTEND -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -DIN_GCC  -DCROSS_DIRECTORY_STRUCTURE  -fno-exceptions -fno-rtti -fasynchronous-unwind-tables -W -Wall -Wno-narrowing -Wwrite-strings -Wcast-qual -Wmissing-format-attribute -pedantic -Wno-long-long -Wno-variadic-macros -Wno-overlength-strings   -DHAVE_CONFIG_H -I. -Icp -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../include -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libcpp/include -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include  -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libdecnumber -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libdecnumber/dpd -I../libdecnumber -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libbacktrace    -o cp/search.o -MT cp/search.o -MMD -MP -MF cp/.deps/search.TPo /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/search.c
g++  -c  -DIN_GCC_FRONTEND -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -DIN_GCC  -DCROSS_DIRECTORY_STRUCTURE  -fno-exceptions -fno-rtti -fasynchronous-unwind-tables -W -Wall -Wno-narrowing -Wwrite-strings -Wcast-qual -Wmissing-format-attribute -pedantic -Wno-long-long -Wno-variadic-macros -Wno-overlength-strings   -DHAVE_CONFIG_H -I. -Icp -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../include -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libcpp/include -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include  -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libdecnumber -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libdecnumber/dpd -I../libdecnumber -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libbacktrace    -o cp/semantics.o -MT cp/semantics.o -MMD -MP -MF cp/.deps/semantics.TPo /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/semantics.c
g++  -c  -DIN_GCC_FRONTEND -isystem/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include -O2 -pipe -DIN_GCC  -DCROSS_DIRECTORY_STRUCTURE  -fno-exceptions -fno-rtti -fasynchronous-unwind-tables -W -Wall -Wno-narrowing -Wwrite-strings -Wcast-qual -Wmissing-format-attribute -pedantic -Wno-long-long -Wno-variadic-macros -Wno-overlength-strings   -DHAVE_CONFIG_H -I. -Icp -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../include -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libcpp/include -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/sysroots/aarch64-linux/usr/include  -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libdecnumber -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libdecnumber/dpd -I../libdecnumber -I/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/../libbacktrace    -o cp/tree.o -MT cp/tree.o -MMD -MP -MF cp/.deps/tree.TPo /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/tree.c
In file included from ./tm.h:24,
                 from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/except.c:27:
/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/config/elfos.h:102:21: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  102 |    fprintf ((FILE), "%s"HOST_WIDE_INT_PRINT_UNSIGNED"\n",\
      |                     ^
/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/config/elfos.h:170:24: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  170 |       fprintf ((FILE), ","HOST_WIDE_INT_PRINT_UNSIGNED",%u\n",  \
      |                        ^
In file included from ./tm.h:38,
                 from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/except.c:27:
././defaults.h:126:24: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  126 |       fprintf ((FILE), ","HOST_WIDE_INT_PRINT_UNSIGNED",%u\n",  \
      |                        ^
In file included from ./tm.h:24,
                 from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/search.c:27:
/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/config/elfos.h:102:21: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  102 |    fprintf ((FILE), "%s"HOST_WIDE_INT_PRINT_UNSIGNED"\n",\
      |                     ^
/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/config/elfos.h:170:24: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  170 |       fprintf ((FILE), ","HOST_WIDE_INT_PRINT_UNSIGNED",%u\n",  \
      |                        ^
In file included from ./tm.h:38,
                 from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/search.c:27:
././defaults.h:126:24: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  126 |       fprintf ((FILE), ","HOST_WIDE_INT_PRINT_UNSIGNED",%u\n",  \
      |                        ^
In file included from ./tm.h:24,
                 from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/semantics.c:29:
/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/config/elfos.h:102:21: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  102 |    fprintf ((FILE), "%s"HOST_WIDE_INT_PRINT_UNSIGNED"\n",\
      |                     ^
/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/config/elfos.h:170:24: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  170 |       fprintf ((FILE), ","HOST_WIDE_INT_PRINT_UNSIGNED",%u\n",  \
      |                        ^
In file included from ./tm.h:24,
                 from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/tree.c:24:
/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/config/elfos.h:102:21: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  102 |    fprintf ((FILE), "%s"HOST_WIDE_INT_PRINT_UNSIGNED"\n",\
      |                     ^
/home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/config/elfos.h:170:24: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  170 |       fprintf ((FILE), ","HOST_WIDE_INT_PRINT_UNSIGNED",%u\n",  \
      |                        ^
In file included from ./tm.h:38,
                 from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/semantics.c:29:
././defaults.h:126:24: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  126 |       fprintf ((FILE), ","HOST_WIDE_INT_PRINT_UNSIGNED",%u\n",  \
      |                        ^
In file included from ./tm.h:38,
                 from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/tree.c:24:
././defaults.h:126:24: warning: invalid suffix on literal; C++11 requires a space between literal and string macro [-Wliteral-suffix]
  126 |       fprintf ((FILE), ","HOST_WIDE_INT_PRINT_UNSIGNED",%u\n",  \
      |                        ^
In file included from /home/ubuntu/development/thirdparties/nxp_yocto/build_ls1046ardb/tmp/work-shared/gcc-linaro-4.9-r2015.03/gcc-linaro-4.9-2015.03/gcc/cp/except.c:1013:
cfns.gperf:101:1: error: 'const char* libc_name_p(const char*, unsigned int)' redeclared inline with 'gnu_inline' attribute
cfns.gperf:26:14: note: 'const char* libc_name_p(const char*, unsigned int)' previously declared here
cfns.gperf:26:14: warning: inline function 'const char* libc_name_p(const char*, unsigned int)' used but never defined
Makefile:1062: recipe for target 'cp/except.o' failed

 

Any pointers on how I should go about solving this?

0 项奖励
回复
1 解答
1,776 次查看
mharshe
Contributor I

I did use those images and ISOs but the I think the problem was with using Ubuntu 16.04. It disappeared when I built inside a docker container running Ubuntu 14.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,777 次查看
mharshe
Contributor I

I did use those images and ISOs but the I think the problem was with using Ubuntu 16.04. It disappeared when I built inside a docker container running Ubuntu 14.

0 项奖励
回复
1,790 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please use NXP formal released QorIQ Linux SDK.

Please download and install following ISOs and tar ball from the link "https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk...

Source: QorIQ Linux SDK v2.0

Update: QorIQ Linux SDK v2.0-1703

0 项奖励
回复