I just starter to work with LS1021A-IOT reference design ...
I have downloaded *.iso file form LS1021A-IoT Gateway Reference Design|Freescale and I’m trying to build fsl-image-full at firs time
and got "ERROR: Task 1083 (virtual:native:/home/<user_directory>/QorIQ-SDK-V1.7-20141218-yocto_RDS_20150302/poky/meta/recipes-devtools/elfutils/elfutils_0.155.bb, do_configure) failed with exit code '1' .
Does someone has idea what may be a problem?
Thanks
In addition, I have tried its virtual machine
but what is a password to run it?
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Pavel
Unfortunately, it does'n solve the problem....
I am trying to use Freescale virtual machine, but its Yocto doesn't support LS1021A-IOT refernce design.
So what I do is installing the fresh QorIQ-SDK-v1.8-SOURCE-20150619-yocto.iso image, trying to compile
It take a long time ( I don't need to tell you, isn't? :smileyhappy: ) . Let's see if it done ...
I will appreciate if I can connect with you by skype... ?
Thanks you
Evgeny
Pavel,
Find out the the recently downloaded QorIQ-SDK-v1.8-SOURCE-20150619-yocto.iso
doesn't include support for LS1021A-IOT ...
Where I can get LS1021A-IOT layer?
Thanks
Evgeny
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------