Hi,
I get an error in the alsa-utils recipe (which I don't care about) when building the SDK 1.7.
ERROR: Task 2239 (/media/wd_3tb/yocto/QorIQ-SDK-V1.7-20141218-yocto/poky/meta/recipes-multimedia/alsa/alsa-utils_1.0.27.2.bb, do_configure) failed with exit code '1'
I'm attaching a log with the verbose output.
Is this a known issue or perhaps something with my environment (Ubuntu 12.04. Building from the SDK source ISO.)?
Thanks
Sidharth
Hello Sidharth Kodikal,
It seems that there is a dependence missing problem in your build environment, please run "bitbake alsa-utils" first, then continue to perform you build, this command will force necessary dependent packages deployed in your build environment.
Please feel free to let me know, if your problem remains.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yiping Wang
i have faced the same problem , and tried the solution you suggested but dint got the problem solved.
ERROR: Task 5 (/home/setu/var-som-mx6-daisy-v7/sources/poky/meta/recipes-multimedia/alsa/alsa-utils_1.0.27.2.bb, do_configure) failed with exit code '1'
here is the error i am facing.