Want to use 5G module on Layerscape platform? The attached Application Notes will help you to do this.
This AN will help you:
1. Set the 5G environment on Layerscape platforms
2. Connect 5G modules to Layerscape platforms.
3. Install the software required for 5G modules and 5G test on
OK1028A-C v1.1 and OK1046A-C2 v1.1 boards. The boards come
from a third-part company, Forlinx, and they can be bought at
https://www.forlinx.com/
4. The test process and the reference result of the test
The patches for 5G modules are based on linux kernel v5.4.49. You may change a little bit if you are not using this kernel.
Have fun with 5G modules.
已解决! 转到解答。
We developed LS1046 based custom card. After assembly we found short in one of NXP LS1046 chip power voltage 1.2V.
Please tell us , what is minimum resistance vale measured between 1.2Voltage and GND for NXP device LS1046.
We developed LS1046 based custom card. After assembly we found short in one of NXP LS1046 chip power voltage 1.2V.
Please tell us , what is minimum resistance vale measured between 1.2Voltage and GND for NXP device LS1046.
Hi ,
We are planning to develop custom board using Layerscape platform LS1046a for 5G CPE application.
we have selected Telit 5G FN980 modem.
Please let us will NXP LS1046 will support & tested with FN980.
Regards,
SUMA ,