i use T2080RDB to compile the program x265. in the directory x265->build->README.txt, i follow the README.txt saying. first, Use cmake to generate Makefiles: cmake ../source; second, build x265: make. but during the make operating,There appears to be a problem.
libx265.so.51: undefined reference to `__sqrtf_finite'
libx265.so.51: undefined reference to `__sqrt_finite'
collect2: error: ld returned 1 exit status
CMakeFiles/cli.dir/build.make:261: recipe for target 'x265' failed
make[2]: *** [x265] Error 1
CMakeFiles/Makefile2:91: recipe for target 'CMakeFiles/cli.dir/all' failed
make[1]: *** [CMakeFiles/cli.dir/all] Error 2
Makefile:116: recipe for target 'all' failed
i hope someone can help me, thank you very much!!!
Hello Jian Zhu,
The function __sqrtf_finite should be provided in libm libarary. Did you include it in your Makefile?
Would you please share your Makefle?
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello, Yiping
firstly thank you for you help!
the following is the Makefile after ./make-Makefiles.bash
# CMAKE generated file: DO NOT EDIT!
# Generated by "Unix Makefiles" Generator, CMake Version 3.2
# Default target executed when no arguments are given to make.
default_target: all
.PHONY : default_target
# Allow only one "make -f Makefile2" at a time, but pass parallelism.
.NOTPARALLEL:
#=============================================================================
# Special targets provided by cmake.
# Disable implicit rules so canonical targets will work.
.SUFFIXES:
# Remove some rules from gmake that .SUFFIXES does not remove.
SUFFIXES =
.SUFFIXES: .hpux_make_needs_suffix_list
# Suppress display of executed commands.
$(VERBOSE).SILENT:
# A target that is always out of date.
cmake_force:
.PHONY : cmake_force
#=============================================================================
# Set environment variables for the build.
# The shell in which to execute make rules.
SHELL = /bin/sh
# The CMake executable.
CMAKE_COMMAND = /home/root/cmake-build-3.2.2/bin/cmake
# The command to remove a file.
RM = /home/root/cmake-build-3.2.2/bin/cmake -E remove -f
# Escaping for special characters.
EQUALS = =
# The top-level source directory on which CMake was run.
CMAKE_SOURCE_DIR = /home/root/x265_1.6/source
# The top-level build directory on which CMake was run.
CMAKE_BINARY_DIR = /home/root/x265_1.6/build/linux
#=============================================================================
# Targets provided globally by CMake.
# Special rule for the target install/strip
install/strip: preinstall
@$(CMAKE_COMMAND) -E cmake_echo_color --switch=$(COLOR) --cyan "Installing the project stripped..."
/home/root/cmake-build-3.2.2/bin/cmake -DCMAKE_INSTALL_DO_STRIP=1 -P cmake_install.cmake
.PHONY : install/strip
# Special rule for the target install/strip
install/strip/fast: install/strip
.PHONY : install/strip/fast
# Special rule for the target edit_cache
edit_cache:
@$(CMAKE_COMMAND) -E cmake_echo_color --switch=$(COLOR) --cyan "Running CMake cache editor..."
/home/root/cmake-build-3.2.2/bin/ccmake -H$(CMAKE_SOURCE_DIR) -B$(CMAKE_BINARY_DIR)
.PHONY : edit_cache
# Special rule for the target edit_cache
edit_cache/fast: edit_cache
.PHONY : edit_cache/fast
# Special rule for the target rebuild_cache
rebuild_cache:
@$(CMAKE_COMMAND) -E cmake_echo_color --switch=$(COLOR) --cyan "Running CMake to regenerate build system..."
/home/root/cmake-build-3.2.2/bin/cmake -H$(CMAKE_SOURCE_DIR) -B$(CMAKE_BINARY_DIR)
.PHONY : rebuild_cache
# Special rule for the target rebuild_cache
rebuild_cache/fast: rebuild_cache
.PHONY : rebuild_cache/fast
# Special rule for the target install
install: preinstall
@$(CMAKE_COMMAND) -E cmake_echo_color --switch=$(COLOR) --cyan "Install the project..."
/home/root/cmake-build-3.2.2/bin/cmake -P cmake_install.cmake
.PHONY : install
# Special rule for the target install
install/fast: preinstall/fast
@$(CMAKE_COMMAND) -E cmake_echo_color --switch=$(COLOR) --cyan "Install the project..."
/home/root/cmake-build-3.2.2/bin/cmake -P cmake_install.cmake
.PHONY : install/fast
# Special rule for the target list_install_components
list_install_components:
@$(CMAKE_COMMAND) -E cmake_echo_color --switch=$(COLOR) --cyan "Available install components are: \"Unspecified\""
.PHONY : list_install_components
# Special rule for the target list_install_components
list_install_components/fast: list_install_components
.PHONY : list_install_components/fast
# Special rule for the target install/local
install/local: preinstall
@$(CMAKE_COMMAND) -E cmake_echo_color --switch=$(COLOR) --cyan "Installing only the local directory..."
/home/root/cmake-build-3.2.2/bin/cmake -DCMAKE_INSTALL_LOCAL_ONLY=1 -P cmake_install.cmake
.PHONY : install/local
# Special rule for the target install/local
install/local/fast: install/local
.PHONY : install/local/fast
# The main all target
all: cmake_check_build_system
$(CMAKE_COMMAND) -E cmake_progress_start /home/root/x265_1.6/build/linux/CMakeFiles /home/root/x265_1.6/build/linux/CMakeFiles/progress.marks
$(MAKE) -f CMakeFiles/Makefile2 all
$(CMAKE_COMMAND) -E cmake_progress_start /home/root/x265_1.6/build/linux/CMakeFiles 0
.PHONY : all
# The main clean target
clean:
$(MAKE) -f CMakeFiles/Makefile2 clean
.PHONY : clean
# The main clean target
clean/fast: clean
.PHONY : clean/fast
# Prepare targets for installation.
preinstall: all
$(MAKE) -f CMakeFiles/Makefile2 preinstall
.PHONY : preinstall
# Prepare targets for installation.
preinstall/fast:
$(MAKE) -f CMakeFiles/Makefile2 preinstall
.PHONY : preinstall/fast
# clear depends
depend:
$(CMAKE_COMMAND) -H$(CMAKE_SOURCE_DIR) -B$(CMAKE_BINARY_DIR) --check-build-system CMakeFiles/Makefile.cmake 1
.PHONY : depend
#=============================================================================
# Target rules for targets named clean-generated
# Build rule for target.
clean-generated: cmake_check_build_system
$(MAKE) -f CMakeFiles/Makefile2 clean-generated
.PHONY : clean-generated
# fast build rule for target.
clean-generated/fast:
$(MAKE) -f CMakeFiles/clean-generated.dir/build.make CMakeFiles/clean-generated.dir/build
.PHONY : clean-generated/fast
#=============================================================================
# Target rules for targets named cli
# Build rule for target.
cli: cmake_check_build_system
$(MAKE) -f CMakeFiles/Makefile2 cli
.PHONY : cli
# fast build rule for target.
cli/fast:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/build
.PHONY : cli/fast
#=============================================================================
# Target rules for targets named uninstall
# Build rule for target.
uninstall: cmake_check_build_system
$(MAKE) -f CMakeFiles/Makefile2 uninstall
.PHONY : uninstall
# fast build rule for target.
uninstall/fast:
$(MAKE) -f CMakeFiles/uninstall.dir/build.make CMakeFiles/uninstall.dir/build
.PHONY : uninstall/fast
#=============================================================================
# Target rules for targets named x265-shared
# Build rule for target.
x265-shared: cmake_check_build_system
$(MAKE) -f CMakeFiles/Makefile2 x265-shared
.PHONY : x265-shared
# fast build rule for target.
x265-shared/fast:
$(MAKE) -f CMakeFiles/x265-shared.dir/build.make CMakeFiles/x265-shared.dir/build
.PHONY : x265-shared/fast
#=============================================================================
# Target rules for targets named x265-static
# Build rule for target.
x265-static: cmake_check_build_system
$(MAKE) -f CMakeFiles/Makefile2 x265-static
.PHONY : x265-static
# fast build rule for target.
x265-static/fast:
$(MAKE) -f CMakeFiles/x265-static.dir/build.make CMakeFiles/x265-static.dir/build
.PHONY : x265-static/fast
#=============================================================================
# Target rules for targets named encoder
# Build rule for target.
encoder: cmake_check_build_system
$(MAKE) -f CMakeFiles/Makefile2 encoder
.PHONY : encoder
# fast build rule for target.
encoder/fast:
$(MAKE) -f encoder/CMakeFiles/encoder.dir/build.make encoder/CMakeFiles/encoder.dir/build
.PHONY : encoder/fast
#=============================================================================
# Target rules for targets named common
# Build rule for target.
common: cmake_check_build_system
$(MAKE) -f CMakeFiles/Makefile2 common
.PHONY : common
# fast build rule for target.
common/fast:
$(MAKE) -f common/CMakeFiles/common.dir/build.make common/CMakeFiles/common.dir/build
.PHONY : common/fast
filters/filters.o: filters/filters.cpp.o
.PHONY : filters/filters.o
# target to build an object file
filters/filters.cpp.o:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/filters/filters.cpp.o
.PHONY : filters/filters.cpp.o
filters/filters.i: filters/filters.cpp.i
.PHONY : filters/filters.i
# target to preprocess a source file
filters/filters.cpp.i:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/filters/filters.cpp.i
.PHONY : filters/filters.cpp.i
filters/filters.s: filters/filters.cpp.s
.PHONY : filters/filters.s
# target to generate assembly for a file
filters/filters.cpp.s:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/filters/filters.cpp.s
.PHONY : filters/filters.cpp.s
input/input.o: input/input.cpp.o
.PHONY : input/input.o
# target to build an object file
input/input.cpp.o:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/input/input.cpp.o
.PHONY : input/input.cpp.o
input/input.i: input/input.cpp.i
.PHONY : input/input.i
# target to preprocess a source file
input/input.cpp.i:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/input/input.cpp.i
.PHONY : input/input.cpp.i
input/input.s: input/input.cpp.s
.PHONY : input/input.s
# target to generate assembly for a file
input/input.cpp.s:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/input/input.cpp.s
.PHONY : input/input.cpp.s
input/y4m.o: input/y4m.cpp.o
.PHONY : input/y4m.o
# target to build an object file
input/y4m.cpp.o:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/input/y4m.cpp.o
.PHONY : input/y4m.cpp.o
input/y4m.i: input/y4m.cpp.i
.PHONY : input/y4m.i
# target to preprocess a source file
input/y4m.cpp.i:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/input/y4m.cpp.i
.PHONY : input/y4m.cpp.i
input/y4m.s: input/y4m.cpp.s
.PHONY : input/y4m.s
# target to generate assembly for a file
input/y4m.cpp.s:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/input/y4m.cpp.s
.PHONY : input/y4m.cpp.s
input/yuv.o: input/yuv.cpp.o
.PHONY : input/yuv.o
# target to build an object file
input/yuv.cpp.o:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/input/yuv.cpp.o
.PHONY : input/yuv.cpp.o
input/yuv.i: input/yuv.cpp.i
.PHONY : input/yuv.i
# target to preprocess a source file
input/yuv.cpp.i:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/input/yuv.cpp.i
.PHONY : input/yuv.cpp.i
input/yuv.s: input/yuv.cpp.s
.PHONY : input/yuv.s
# target to generate assembly for a file
input/yuv.cpp.s:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/input/yuv.cpp.s
.PHONY : input/yuv.cpp.s
output/output.o: output/output.cpp.o
.PHONY : output/output.o
# target to build an object file
output/output.cpp.o:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/output/output.cpp.o
.PHONY : output/output.cpp.o
output/output.i: output/output.cpp.i
.PHONY : output/output.i
# target to preprocess a source file
output/output.cpp.i:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/output/output.cpp.i
.PHONY : output/output.cpp.i
output/output.s: output/output.cpp.s
.PHONY : output/output.s
# target to generate assembly for a file
output/output.cpp.s:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/output/output.cpp.s
.PHONY : output/output.cpp.s
output/y4m.o: output/y4m.cpp.o
.PHONY : output/y4m.o
# target to build an object file
output/y4m.cpp.o:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/output/y4m.cpp.o
.PHONY : output/y4m.cpp.o
output/y4m.i: output/y4m.cpp.i
.PHONY : output/y4m.i
# target to preprocess a source file
output/y4m.cpp.i:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/output/y4m.cpp.i
.PHONY : output/y4m.cpp.i
output/y4m.s: output/y4m.cpp.s
.PHONY : output/y4m.s
# target to generate assembly for a file
output/y4m.cpp.s:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/output/y4m.cpp.s
.PHONY : output/y4m.cpp.s
output/yuv.o: output/yuv.cpp.o
.PHONY : output/yuv.o
# target to build an object file
output/yuv.cpp.o:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/output/yuv.cpp.o
.PHONY : output/yuv.cpp.o
output/yuv.i: output/yuv.cpp.i
.PHONY : output/yuv.i
# target to preprocess a source file
output/yuv.cpp.i:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/output/yuv.cpp.i
.PHONY : output/yuv.cpp.i
output/yuv.s: output/yuv.cpp.s
.PHONY : output/yuv.s
# target to generate assembly for a file
output/yuv.cpp.s:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/output/yuv.cpp.s
.PHONY : output/yuv.cpp.s
x265.o: x265.cpp.o
.PHONY : x265.o
# target to build an object file
x265.cpp.o:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/x265.cpp.o
.PHONY : x265.cpp.o
x265.i: x265.cpp.i
.PHONY : x265.i
# target to preprocess a source file
x265.cpp.i:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/x265.cpp.i
.PHONY : x265.cpp.i
x265.s: x265.cpp.s
.PHONY : x265.s
# target to generate assembly for a file
x265.cpp.s:
$(MAKE) -f CMakeFiles/cli.dir/build.make CMakeFiles/cli.dir/x265.cpp.s
.PHONY : x265.cpp.s
# Help Target
help:
@echo "The following are some of the valid targets for this Makefile:"
@echo "... all (the default if no target is provided)"
@echo "... clean"
@echo "... depend"
@echo "... install/strip"
@echo "... x265-static"
@echo "... uninstall"
@echo "... edit_cache"
@echo "... rebuild_cache"
@echo "... cli"
@echo "... install"
@echo "... list_install_components"
@echo "... x265-shared"
@echo "... clean-generated"
@echo "... install/local"
@echo "... encoder"
@echo "... common"
@echo "... filters/filters.o"
@echo "... filters/filters.i"
@echo "... filters/filters.s"
@echo "... input/input.o"
@echo "... input/input.i"
@echo "... input/input.s"
@echo "... input/y4m.o"
@echo "... input/y4m.i"
@echo "... input/y4m.s"
@echo "... input/yuv.o"
@echo "... input/yuv.i"
@echo "... input/yuv.s"
@echo "... output/output.o"
@echo "... output/output.i"
@echo "... output/output.s"
@echo "... output/y4m.o"
@echo "... output/y4m.i"
@echo "... output/y4m.s"
@echo "... output/yuv.o"
@echo "... output/yuv.i"
@echo "... output/yuv.s"
@echo "... x265.o"
@echo "... x265.i"
@echo "... x265.s"
.PHONY : help
#=============================================================================
# Special targets to cleanup operation of make.
# Special rule to run CMake to check the build system integrity.
# No rule that depends on this can have commands that come from listfiles
# because they might be regenerated.
cmake_check_build_system:
$(CMAKE_COMMAND) -H$(CMAKE_SOURCE_DIR) -B$(CMAKE_BINARY_DIR) --check-build-system CMakeFiles/Makefile.cmake 0
.PHONY : cmake_check_build_system