Hi experts,
When I test EDAC on nxp-ls1028ardb board with LSDK20.04 v4.19 kernel opening EDAC_DEBUG, the dmesg shows followings:
root@localhost:~# uname -a
Linux localhost 4.19.90 #4 SMP PREEMPT Tue Jul 21 19:22:26 CST 2020 aarch64 aarch64 aarch64 GNU/Linux
root@localhost:~# 
root@localhost:~# dmesg | grep EDAC
[ 1.768901] EDAC MC: Ver: 3.0.0
[ 1.772125] EDAC DEBUG: edac_mc_sysfs_init: device mc created
[ 3.658749] EDAC DEBUG: edac_mc_alloc: allocating 1928 bytes for mci data (4 ranks, 4 csrows/channels)
[ 3.663852] EDAC DEBUG: edac_mc_free: 
root@localhost:~# 
root@localhost:~# dmesg | grep ECC 
[ 3.658776] fsl_mc_err_probe: No ECC DIMMs discovered
[ 9.880553] systemd[1]: systemd 237 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID )
root@localhost:~# 
root@localhost:~#
But I see the U-boot shows
DRAM: 3.9 GiB
DDR 3.9 GiB (DDR4, 32-bit, CL=11, ECC on)
And the user manual of ls1028 board says that it supports ECC.
So I want to query if there any known issue about ECC and EDAC?
Thanks,
Zhantao
Hello zhantao,
The driver file drivers/edac/fsl_ddr_edac.c is not suitable for LS1028 platform, it's used for PowerPC platform.
Thanks,
Yiping
Hi Yiping,
Thanks for your reply.
That is to say, all the arm64 processor based products like nxp LS-series do not support EDAC?
Thanks,
Zhantao
For Layerscape platform, please configure the following in Linux Kernel.
CONFIG_EDAC_DEBUG=y
CONFIG_EDAC_LAYERSCAPE=y
Hi Yiping,
I have add all the following configs:
root@nxp-ls1028:~# zcat /proc/config.gz | grep EDAC
CONFIG_EDAC_SUPPORT=y
CONFIG_EDAC=y
CONFIG_EDAC_LEGACY_SYSFS=y
CONFIG_EDAC_DEBUG=y
CONFIG_EDAC_LAYERSCAPE=y
And the result is as what I stated.
Thanks,
Zhantao
Please configure ECC as the following in u-boot, then do EDAC verification.
=> setenv hwconfig fsl_ddr:ecc=on
Hi Yiping,
Thanks for your reply.
It seems even set hwconfig fsl_ddr:ecc=on in U-boot, the EDAC still not work.
Welcome to NXP LSDK 2004 main (GNU/Linux 4.19.90 aarch64)
* Support: https://www.nxp.com/lsdk
 * Documentation: https://lsdk.github.io/document
 * Licensing: https://lsdk.github.io/eula
root@localhost:~# dmesg | grep EDAC
[ 1.764898] EDAC MC: Ver: 3.0.0
[ 1.768120] EDAC DEBUG: edac_mc_sysfs_init: device mc created
[ 3.654712] EDAC DEBUG: edac_mc_alloc: allocating 1928 bytes for mci data (4 ranks, 4 csrows/channels)
[ 3.659814] EDAC DEBUG: edac_mc_free: 
root@localhost:~# 
root@localhost:~# dmesg | grep ECC 
[ 3.654738] fsl_mc_err_probe: No ECC DIMMs discovered
[ 9.954633] systemd[1]: systemd 237 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID )
root@localhost:~# 
root@localhost:~# uname -a
Linux localhost 4.19.90 #4 SMP PREEMPT Tue Jul 21 19:22:26 CST 2020 aarch64 aarch64 aarch64 GNU/Linux
root@localhost:~#
Thanks,
Zhantao
Hello Zhantao,
I didn't reproduce this issue on LS1046ARDB and LS1088ARDB, this problem should be caused by EDAC driver not compatible with LS1028ARDB platform. I have reported this issue to the development team to do more investigation.
Thanks,
Yiping
Hi Yiping,
Thanks a lot.
Please let me know if there is any progress.
Thanks,
Zhantao