Driving TFT LCD 800x400 with LS1012A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Driving TFT LCD 800x400 with LS1012A

985 Views
nuttakorntrirat
Contributor II

Do I need to add what external chips if I use LS1012A to driving TFT LCD?

Labels (1)
3 Replies

801 Views
nuttakorntrirat
Contributor II

Hi Serguei, 

                Many thank, Could you show an example to use LS1012A to drive TFT LCD? 

0 Kudos

801 Views
r8070z
NXP Employee
NXP Employee

Yes you need for external TFT LCD controller in-between LS1021A and TFT LCD panel. There are TFT LCD controllers with SPI and I2C interfaces, so you may add TFT LCD controller to LS1012A SPI interface.

801 Views
nuttakorntrirat
Contributor II

Hi team, 

             I just know I may need to add grachic processing/ display controller via SPI interface. right ?

Thank for any comment.

Nut 

0 Kudos