Does the LS1012ARDB support SD UHS-I?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the LS1012ARDB support SD UHS-I?

Jump to solution
999 Views
zalbassam
Contributor I

Hi,

Iam trying to check the performance of the SD card on the LS1012ARDB, using a Sandisk Extreme Pro UHS-I sd card.

When I check the AUTOCERR_SYSCTL2 register of the esdhc1 I see the UHSM field is set to SDR12 (with and without data transfer):

root@OpenWrt:/mnt# devmem 0x156003c
0x00000000

The manual says that the LS1012A itself supports SDR104. My question is, does the RDB supports UHS-I mode? if yes how to switch the Linux driver to use it?

Thank you,

Zaid

Labels (1)
0 Kudos
1 Solution
849 Views
Pavel
NXP Employee
NXP Employee

Look at the following page:

https://community.nxp.com/thread/447129

 

It looks like that changing of the LS1012a driver code is needed as solution for this problem.


Have a great day,
Pavel Chubakov
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
850 Views
Pavel
NXP Employee
NXP Employee

Look at the following page:

https://community.nxp.com/thread/447129

 

It looks like that changing of the LS1012a driver code is needed as solution for this problem.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos