Does an LS1028A-family SoC without encryption support Secure Boot or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does an LS1028A-family SoC without encryption support Secure Boot or not?

828 Views
jclsn
Contributor IV

I am currently trying to implmement Secure Boot for an LS1017A. I discovered that the SoC is labeled as "without encryption". In the LS1028A Security Reference Manual section 3.2 it says that the CHA (Cryptographic hardware acceleration) module still supports some basic algortihms also on SoCs without encryption.

I am a bit unsure now if this module is necessary for Secure Boot or what the difference to the CAAM module is.

In any case, I would like to know: Is Secure boot is still possible on devices labeled as "without encryption"?

0 Kudos
Reply
2 Replies

779 Views
kenli
NXP Employee
NXP Employee

For secure boot to work, customer needs to order the "E" version, which has the SEC engine enabled. The non-"E" part does not work with secure boot.and this condition applies to all layerscape series.
ls1028a.png

 

Best regards
0 Kudos
Reply

800 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hello @jclsn,

I would like to inform you that I'm working on your question, I will let you know as soon as I have an update.

Thank you so much for your patience

Regards,

Sebastian

0 Kudos
Reply