Display Clock Frequency in U-Boot for LS1043ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Display Clock Frequency in U-Boot for LS1043ARDB

Jump to solution
965 Views
aismail102
Contributor II

How do I display the CPU clock frequencies in U-Boot? CMD_CLK is deprecated and the only other cmd that possibly displays this information is CMD_CPU, however, enabling CMD_CPU causes U-Boot not to build. Is there a command available that I can enable that will display the clock frequencies?

Labels (2)
0 Kudos
1 Solution
951 Views
Pavel
NXP Employee
NXP Employee

See attached snapshot. This snapshot shows that u-boot reports CPUx clock, Bus clock, DDR clock and FMAN clock on the LS1043a board.

Is additional clock needed to show?

View solution in original post

0 Kudos
1 Reply
952 Views
Pavel
NXP Employee
NXP Employee

See attached snapshot. This snapshot shows that u-boot reports CPUx clock, Bus clock, DDR clock and FMAN clock on the LS1043a board.

Is additional clock needed to show?

0 Kudos