Disable 10G port on LS1043ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable 10G port on LS1043ARDB

492 Views
ts1234
Contributor III

I am facing a high temperature issue on 10G heatsink.  I want to test this board with 10G port disabled (both in uboot and kernel).

How do I permanently disable the 10G port on LS1043ARDB?

 

 

0 Kudos
1 Reply

485 Views
yipingwang
NXP TechSupport
NXP TechSupport
Please refer to section "32.1.1.2 SerDes protocols" in LS1043A Reference Manual, you could configure RCW filed SRDS_PRTCL_S1(RCW[128:143]) as "2455" to replace the default value "1455" to disable XFI.m9(10G port).
0 Kudos