DPDK folder not Present : LSDK 21.08 on LX2160

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DPDK folder not Present : LSDK 21.08 on LX2160

Jump to solution
1,171 Views
Chidananda22
Contributor III

Hi ,

in one of customer provided LS2160 HW dpdk was not packaged in rfs on this hardware.

Can you please suggest it is fine if copy the folder from different LS2160 with LSDK 21.08 .

Or I need to proceed some different steps. As I can't reflash the full LSDK again.

 

0 Kudos
Reply
1 Solution
1,141 Views
yipingwang
NXP TechSupport
NXP TechSupport

You have to rebuild dpdk into rootfs in LSDK 21.08.

flex-builder -c openssl -a arm64 # to resolve the dependency on OpenSSL package
flex-builder -c linux -a arm64 # to resolve the dependency of KNI module
flex-builder -c dpdk -a arm64 # build dpdk application
flex-builder -c pktgen_dpdk -a arm64 # to generate dpdk pktgen application
flex-builder -c ovs_dpdk # to generate ovs-dpdk binaries
flex-builder -i merge-component -a arm64

flex-builder -i packrfs -r ubuntu:main

View solution in original post

2 Replies
1,135 Views
Chidananda22
Contributor III

Thank You .

0 Kudos
Reply
1,142 Views
yipingwang
NXP TechSupport
NXP TechSupport

You have to rebuild dpdk into rootfs in LSDK 21.08.

flex-builder -c openssl -a arm64 # to resolve the dependency on OpenSSL package
flex-builder -c linux -a arm64 # to resolve the dependency of KNI module
flex-builder -c dpdk -a arm64 # build dpdk application
flex-builder -c pktgen_dpdk -a arm64 # to generate dpdk pktgen application
flex-builder -c ovs_dpdk # to generate ovs-dpdk binaries
flex-builder -i merge-component -a arm64

flex-builder -i packrfs -r ubuntu:main