DDRv tool fails due to other DDR hardware or software issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDRv tool fails due to other DDR hardware or software issues

2,131 Views
Rinke
Contributor II

Hi,

Im working on the bringup of our own custom board. Its heavily based on the Freeway LS1046A design. The board boots BL2, DDR controller initializes and boots u-boot. All HW is thus working we conclude. Writing to DDR from U-boot works fine. However we would like to tune the ddr settings using the ddrv tool. But it does not want to work. To make sure the settings are all the same i have created a new project and imported the settings from the board. Exporting these settings and putting them into the init file and checking with connection diagnostics results in all checks OK. So DDR settings should be fine right?

When running the ddrv tool it just does not want to work. The first test we want to try and run is the leveling test. See QCVS and ccs log attached. 

What could I be doing wrong that the DDRv tool is not working? I tried to ignore the ACE error to see if I can get past it. But that doesnt solve the issue. Just different output. 

 

 

0 Kudos
Reply
26 Replies

1,518 Views
June_Lu
NXP TechSupport
NXP TechSupport

Yes, you could read out the uboot values and do the validation, the some bits of wrlv1 wrlvl 2 and 3 would change.

But where the uboot values come from? Many differences from the frwyls1046 values.

Why don't use frwyls1046 value but change the row and col?

What's the DDR data rate?

Thanks

 

0 Kudos
Reply

1,712 Views
June_Lu
NXP TechSupport
NXP TechSupport

From your DDR registers DQ_MAP0, it seems, you have done bit swizzling.

And DDR1_DDR_SDRAM_CFG has obvious error, ECC_EN is not enabled.

So the layout and the DDR part number both different from the Freeway LS1046A design.

Would you provide the info:

- DDR data sheet.

- DDR schematics.

- the snapshot of QCVS "New QorIQ Configuration Guide" -> "DDR configuration" page to check if the DDR SW configurations match the DDR hardware.

Another good reference, after you boot in the uboot, connect the CW read out all related DRAM registers:

(bin) 2 % delete all

(bin) 3 % config cc cwtap:10.193.20.35

(bin) 4 % show cc

0: CodeWarrior TAP (cwtap:10.193.20.35) CC software ver. {0.0}

(bin) 5 % ccs::config_chain {ls1043a dap sap2}

(bin) 6 % ccs::display_mem 32 0x1080100 4 0 4

Read all the related registers,  and compare the registers you configured when do the validation.

June_Lu_0-1741947336097.png

 

0 Kudos
Reply

1,688 Views
Rinke
Contributor II

From your DDR registers DQ_MAP0, it seems, you have done bit swizzling.

We dont do bit swizzling. All are connected in order. We have also tried to leave DQ_MAP at default. Does not make a difference. But we tried to set them in order to check if it makes a difference.  I have attached our latest ddr config. This is exported from the board and fully working. Except ddrv then. 

And DDR1_DDR_SDRAM_CFG has obvious error, ECC_EN is not enabled.

When I check ECC_EN is actually enabled in the configuration registers view. 

Screenshot 2025-03-14 200731.png

So the layout and the DDR part number both different from the Freeway LS1046A design.

Yes true in some way its different. But most other parts are the same. Clock design, flash etc. 

Would you provide the info:

DDR data sheet.

- DDR schematics.

Both see attached

- the snapshot of QCVS "New QorIQ Configuration Guide" -> "DDR configuration" page to check if the DDR SW configurations match the DDR hardware.

Will upload screenshot later

Another good reference, after you boot in the uboot, connect the CW read out all related DRAM registers:

(bin) 2 % delete all

(bin) 3 % config cc cwtap:10.193.20.35

(bin) 4 % show cc

0: CodeWarrior TAP (cwtap:10.193.20.35) CC software ver. {0.0}

(bin) 5 % ccs::config_chain {ls1043a dap sap2}

(bin) 6 % ccs::display_mem 32 0x1080100 4 0 4

Read all the related registers,  and compare the registers you configured when do the validation.

Thanks. I have attached output from ccs ddr registers after uboot booting and after running the wrlvl test. I do see some differences but not sure if any major ones. wrlvl 2 and 3 are set to 0? But this is part of the test I think?

 

0 Kudos
Reply

1,923 Views
June_Lu
NXP TechSupport
NXP TechSupport

Have you followed the QCVS_DDR_User_Guide to configure the DDR parameters.

Have you followed the AN5097, Hardware and Layout Design Considerations for DDR4 SDRAM Memory Interfaces when do the layout?

If your DDR part number and config are all same as Freeway LS1046A design,  you could use the configuration of the Freeway LS1046A first.

Any difference, you should adjust the parameters.

0 Kudos
Reply

1,868 Views
Rinke
Contributor II

Hey,

Yes we have followed those guides. Again, the board is able to boot into U-boot with DDR working. So we have a config that should work fine. But using this exact config to run the DDRv tool it does not seem to work. DDR part number is different from Freeway. But again we changed those settings and DDR U-boot is working. So all good. 

Any tips to check why DDRv is not able to be ran?

0 Kudos
Reply

1,806 Views
June_Lu
NXP TechSupport
NXP TechSupport

Please confirm your DDR part number and registers you changed per Freeway LS1046A design.

You could share the information here.

 AN5097, Hardware and Layout Design Considerations for DDR4 SDRAM Memory Interfaces should be followed as the layout reference.

0 Kudos
Reply

1,759 Views
Rinke
Contributor II

Hi June,

Yes we followed all the guidelines. You can find my exact configuration in the first post. We are using 5x MT40A1G16TB. One for ECC. 8gb of ram in total. Only 1 chip select. 

The configuration we have is working fine. We can boot into u-boot etc. Connection diagnostics works fine.

 

Screenshot 2025-03-13 211630.png

DDR checks pass. Please help me in getting WRLVL tool to work. I dont understand why it hangs on reading register 0x01080114. See first post for full output including ccs logs. 

read_memory(coreh.{serverh=0,cc_index=0,chain_pos=17},
  addr.{addr_hi=0x00000000,addr_lo=0x01080114,size=4,space=4607},count=4,*data)
  data: 00401030

  

0 Kudos
Reply

1,234 Views
tzaman
Contributor I

Juno, have you had the time to review what Rinke sent? In case it helps, this is ddr_init.c we use in ATF:

#include <assert.h>
#include <errno.h>
#include <string.h>

#include <common/debug.h>
#include <ddr.h>
#include <lib/utils.h>

#include <errata.h>
#include <platform_def.h>

const struct ddr_cfg_regs static_1600 = {
	.cs[0].bnds = 0x1FF,
	.cs[0].config = 0x80840512,
	.cs[0].config_2 = 0x00,
	.timing_cfg[0] = 0x80550018,
	.timing_cfg[1] = 0xCDC60F44,
	.timing_cfg[2] = 0x0049111C,
	.timing_cfg[3] = 0x01161000, 
	.timing_cfg[4] = 0x01,
	.timing_cfg[5] = 0x04001000,
	.timing_cfg[7] = 0x23300000,
	.timing_cfg[8] = 0x03336800, 
	.sdram_cfg[0] = 0xE5040008, // 4 stands for 8-beat bursts
	.sdram_cfg[1] = 0x00400000,
	.dq_map[0] = 0x00,
	.dq_map[1] = 0x00,
	.dq_map[2] = 0x00,
	.dq_map[3] = 0x00,
	.sdram_mode[0] = 0x01010210,
	.sdram_mode[8] = 0x0500,
	.sdram_mode[9] = 0x04C80000,
	.md_cntl = 0x00,
	.interval = 0x18600618,
	.data_init = 0xDEADBEEF, 
	.clk_cntl = 0x02800000,
	.init_addr = 0x00, 
	.ddr_sr_cntr = 0x0, 
	.init_ext_addr = 0x00,
	.zq_cntl = 0x8A090705,
	.wrlvl_cntl[0] = 0x86750603,
	.wrlvl_cntl[1] = 0x03080809,
	.wrlvl_cntl[2] = 0x09090908,
	.cdr[0] = 0x80040000,
	.cdr[1] = 0x81,
	.debug[28] = 0x37
};

long long board_static_ddr(struct ddr_info *priv)
{
	memcpy(&priv->ddr_reg, &static_1600, sizeof(static_1600));

	return 0x200000000;
}

long long init_ddr(void)
{
	int spd_addr[] = { NXP_SPD_EEPROM0 };
	struct ddr_info info;
	struct sysinfo sys;
	long long dram_size;

	zeromem(&sys, sizeof(sys));
	get_clocks(&sys);

	debug("platform clock %lu\n", sys.freq_platform);
	debug("DDR PLL1 %lu\n", sys.freq_ddr_pll0);
	debug("DDR PLL2 %lu\n", sys.freq_ddr_pll1);

	zeromem(&info, sizeof(struct ddr_info));
	info.num_ctlrs = 1;
	info.dimm_on_ctlr = 1;
	info.clk = get_ddr_freq(&sys, 0);
	info.spd_addr = spd_addr;
	info.ddr[0] = (void *)NXP_DDR_ADDR;

	dram_size = dram_init(&info);

	if (dram_size < 0)
		ERROR("DDR init failed.\n");

	erratum_a008850_post();

	return dram_size;
}

 

This code gets us both to u-boot, and further into Linux, which is where stress tests start to fail because obviously, DDR4 is not centred correctly.

 

0 Kudos
Reply

1,080 Views
June_Lu
NXP TechSupport
NXP TechSupport

Please create a new post to address your issue, thanks

0 Kudos
Reply

1,072 Views
tzaman
Contributor I
I don't understand. Why do I need to create a new post. Rinke and me are working on the same board, it's the exact same issue, I'm just providing additional information.
0 Kudos
Reply

1,050 Views
June_Lu
NXP TechSupport
NXP TechSupport

I am sorry, I find your email address is different from the Rinke's.

And the ddr_init.c file misses the struct dimm_params ddr_raw_timing = {. Which is an important part.

Would you follow my comments 2 weeks before:

You could read out the uboot values and do the validation, the some bits of wrlv1 wrlvl 2 and 3 would change.

But where the uboot values come from? Many differences from the frwyls1046 values.

Why don't use frwyls1046 value but change the row and col?

What's the DDR data rate?

I attached the frwyls1046 CodeWarrior value for you refer.

Please find the LSDK2108 frwyls1046 ddr_init.c  below

https://github.com/nxp-qoriq/atf/blob/LSDK-21.08/plat/nxp/soc-ls1046a/ls1046afrwy/ddr_init.c

It's better to update the register with the mode I send to Rinke.

The CodeWarrior window will also be OK.

Thanks

0 Kudos
Reply

1,012 Views
tzaman
Contributor I

Hi June, I think showing you a video will be faster.

As you can see, I can successfully boot into Linux on the board we're bringing up. Reset works properly as well.

Then I load the DDR register values from this very same running board and try validation, which fails.

I don't understand we need the other part (dimm_params ddr_raw_timing), we're using the static configuration so this part doesn't get compiled in.

Interestingly enough, if I take the generated code that CodeWarrior gives me based on this configutation, and in fact use what you're suggesting (set CONFIG_STATIC_DDR to 0), the board doesn't boot. The generated code is quite confusing, and likely wrong.

So the question remains:

Why can we boot into Linux on this board (over and over again, it's not a one-off thing), but when trying to validate DDR, not a single value gets successfully written to DDR?

Thank you.

 

0 Kudos
Reply

985 Views
tzaman
Contributor I

One further observation. I looked at the process that validation tool uses to do the write leveling tests (and all others I assume). 

Once it resets the controller, it checks register 0x01080F04 and in the case of RDB (which we have), this register returns 0x00000002 and the validator then proceeds to test the memory.

In our case, on the other hand, the register 0x01080F04 returns 0x00003002 which I believe makes the tool not to proceed with actual tests. Is there a way for us to learn what this register means?

Here's the debug register values that I get when I read them in u-boot, on the actual board that DDR centering tests are failing:

=> md 0x01080F00
01080f00: 00000000 02300000 0d000000 200c0014  ......0........
01080f10: 00000000 00000000 00000000 00000000  ................
01080f20: 00000000 10101010 10101010 10101010  ................
01080f30: 10101010 00301010 00000000 00000000  ......0.........
01080f40: 00000000 00000000 01000000 000000d4  ................
01080f50: 000b000c 000f000e 00120012 00140012  ................
01080f60: 00000010 00900000 20000000 00000000  ........... ....
01080f70: 37007000 00000000 00000000 00000000  .p.7............
01080f80: 00000000 00000000 00000000 00000000  ................
01080f90: 00000000 00000080 00000000 0030002f  ............/.0.
01080fa0: 002f0030 0030002f 0030002e 0000002f  0././.0...0./...
01080fb0: 03000000 1d1c1c1f 0e1e1d0e 0f0f1d1f  ................
01080fc0: 1d1e1e1e 1e1d1e1f 1d1e1d1d 1f1e1f1f  ................
01080fd0: 1d1f1f1e 1d1a1d1f 1b1c1e1c 1e1b1e1f  ................
01080fe0: 1d1e1f1e 0d1c0d1f 1b1c1e1d 1f1c1f1f  ................
01080ff0: 1d1f201e 1c1a1e1f 1b1c1e1c 0033001f  . ............3.

 

You can see F04 being set to 02300000, which is the same value, written in little endian. 

Is there a way we could investigate this register, or have an idea why it is set to this particular value?

And please don't respond with "F04 is not a public register" because that gives me nothing to investigate further.

Thanks!

0 Kudos
Reply

970 Views
tzaman
Contributor I

I've gotten a bit further in my understanding.

If in u-boot, I check 0x01080E40, I can see that ACE bit is set (which is why I believe F04 is set the way it is, but I might be wrong):

=> md 0x01080E40
01080e40: 80000000 00000000 1d000000 00000000  ................

 

I was under the impression that ACE bit being set would prevent u-boot (let alone Linux kernel) to successfully boot.

This is even more confusing because we can successfully write and read to any offset on the memory, in u-boot, from 0-8GB and get a successful match.

Please advise.

0 Kudos
Reply

882 Views
June_Lu
NXP TechSupport
NXP TechSupport

Have you follow the atf of frwy-ls1046a, setting

# DDR Compilation Configs

CONFIG_STATIC_DDR := 0

CONFIG_DDR_NODIMM := 1

https://github.com/nxp-qoriq/atf/blob/lf-6.6.52-2.2.0/plat/nxp/soc-ls1046a/ls1046afrwy/platform.mk#L...

As the discrete DRAM, CONFIG_DDR_NODIMM := 1 will be set, CONFIG_STATIC_DDR := 0 always should be CONFIG_STATIC_DDR := 0

From your description, it seems the issue is still the getting available parameters of DDR.

That is possible that the board could bring up but could not pass the QCVS, the parameters would be not so reliable. Please adjust the parameters follow my comments before to find a reliable parameters.

Follow the

QCVS_DDR_User_Guide

If you are using discrete DRAM, ensure the filled parameters (DRAM configuration per device, data rate, data bus width, Rank/CS, tCL, tRP/tRCD, ECC enabled) match with the actual DRAM device soldered on the custom board.

How do you set the tCL, tRP/tRCD?

0 Kudos
Reply

753 Views
tzaman
Contributor I

June, we have read QCVS guide at least 20 times now, just to make sure we didn't miss anything.

We cannot just copy over FRWY configuration, because we have different chips and run those at 1600MT/s. If I try (and change values to reflect our chips), I get:

ERROR:   Found training error(s): 0x2000
ERROR:   Error: Waiting for D_INIT timeout.
ERROR:   Writing DDR register(s) failed
ERROR:   Programming DDRC error
ERROR:   DDR init failed.
INFO:    SoC workaround for Errata A008850 Post-Phase was applied
INFO:    RCW BOOT SRC is QSPI
NOTICE:  BL2: v2.10.0   (debug):lf-6.6.52-2.2.0-3-g0d99e2841-dirty
NOTICE:  BL2: Built : 02:21:11, Apr 10 2025
ERROR:   Asserting as the DDR is not initialized yet.ASSERT: plat/nxp/common/setup/ls_bl2_el3_setup.c:285
BACKTRACE: START: assert
0: EL3: 0x10000c00
1: EL3: 0x10007690
2: EL3: 0x10006cf8
3: EL3: 0x10000b38
4: EL3: 0x100000c4
BACKTRACE: END: assert

 

Why does it matter whether CONFIG_STATIC_DDR  is set to 0 or 1? Both ways just configure the DDR controller on the chip no? Yiping said it's fine to use one or the other.

If I take our working configuration, generate ddr_init.h and try to run the settings, with CONFIG_STATIC_DDR set to 0 - then the board doesn't even boot! For some reason, it exports settings for 4GB configuration, despite the fact we have set 8 in QCVS. That is wrong!

Our tCL, tRP/tRCD are all set to 12 clocks.

0 Kudos
Reply

626 Views
June_Lu
NXP TechSupport
NXP TechSupport

Talked with Yiping, yes, when you set the CONFIG_STATIC_DDR to 1 could bring up the board, you could use it.

Although  that is not official supported by the LSDK, but some customers have used it.

Please kindly do the DDR validation start with parameters below instead of parameters from the U-boot:

 

June_Lu_2-1744365024179.png

In the Properties, change the DQ mapping setting below:

 

June_Lu_3-1744365044516.png

Then do the validation.

Please share the screen shots of more settings of DDR configuration options and share the generated QCVS error report(HTML format) if QCVS validations still failed.

0 Kudos
Reply

621 Views
tzaman
Contributor I

Following your suggestion, I get nothing but errors. I don't know how to export QCVS in HTML format. The register dump gives this:

Err. capture registers:
0xE20, 0x00000000     0xE24, 0x00000000     0xE28, 0x00000000     0xE40, 0x00000080     
0xE44, 0x00000100     0xE48, 0x0000001D     0xE4C, 0x00000000     0xE50, 0x00000000     
0xE54, 0x00000000     0xE58, 0x00010000     


Dump:
0xF00, 0x00000000     0xF04, 0x00003100     0xF08, 0x0000000D     0xF0C, 0x14000C20     
0xF10, 0x00000000     0xF14, 0x00000000     0xF18, 0x00000000     0xF1C, 0x00000000     
0xF20, 0x00000000     0xF24, 0x10101010     0xF28, 0x10101010     0xF2C, 0x10101010     
0xF30, 0x10101010     0xF34, 0x10104000     0xF38, 0x00000000     0xF3C, 0x00000000     
0xF40, 0x00000000     0xF44, 0x00000000     0xF48, 0x00000001     0xF4C, 0x11000000     
0xF50, 0x3C003B00     0xF54, 0x3E003F00     0xF58, 0x32003200     0xF5C, 0x32003400     
0xF60, 0x38000000     0xF64, 0x00009000     0xF68, 0x00000020     0xF6C, 0x00000000     
0xF70, 0x0070006F     0xF74, 0x00000000     0xF78, 0x00000000     0xF7C, 0x00000000     
0xF80, 0x00000000     0xF84, 0x00000000     0xF88, 0x00000000     0xF8C, 0x00000000     
0xF90, 0x00000000     0xF94, 0x80000000     0xF98, 0x00000000     0xF9C, 0x00000000     
0xFA0, 0x00000000     0xFA4, 0x00000000     0xFA8, 0x00000000     0xFAC, 0x00000000     
0xFB0, 0x00000000     0xFB4, 0x00000000     0xFB8, 0x00000000     0xFBC, 0x00000000     
0xFC0, 0x00000000     0xFC4, 0x00000000     0xFC8, 0x00000000     0xFCC, 0x00000000     
0xFD0, 0x00000000     0xFD4, 0x00000000     0xFD8, 0x00000000     0xFDC, 0x00000000     
0xFE0, 0x00000000     0xFE4, 0x00000000     0xFE8, 0x00000000     0xFEC, 0x00000000     
0xFF0, 0x00000000     0xFF4, 0x00000000     0xFF8, 0x00000000     0xFFC, 0x00000500

 

You can find screenshots of all of our settings from running the test you suggested attached.

0 Kudos
Reply

617 Views
tzaman
Contributor I

If it helps, these are the registers from our bootable board, when trying to run validation:

Err. capture registers:
0xE20, 0x00000000     0xE24, 0x00000000     0xE28, 0x00000000     0xE40, 0x00000080     
0xE44, 0x00000000     0xE48, 0x00000000     0xE4C, 0x00000000     0xE50, 0x00000000     
0xE54, 0x00000000     0xE58, 0x00000000     


Dump:
0xF00, 0x00000000     0xF04, 0x00003102     0xF08, 0x0000000D     0xF0C, 0x14000C20     
0xF10, 0x00000000     0xF14, 0x00000000     0xF18, 0x00000000     0xF1C, 0x00000000     
0xF20, 0x00000000     0xF24, 0x10101010     0xF28, 0x10101010     0xF2C, 0x10101010     
0xF30, 0x10101010     0xF34, 0x10104000     0xF38, 0x00000000     0xF3C, 0x00000000     
0xF40, 0x00000000     0xF44, 0x00000000     0xF48, 0x00000001     0xF4C, 0x94000000     
0xF50, 0x3C003B00     0xF54, 0x3E003F00     0xF58, 0x32003200     0xF5C, 0x32003400     
0xF60, 0x38000000     0xF64, 0x00009000     0xF68, 0x00000020     0xF6C, 0x00000000     
0xF70, 0x0070006F     0xF74, 0x00000000     0xF78, 0x00000000     0xF7C, 0x00000000     
0xF80, 0x00000000     0xF84, 0x00000000     0xF88, 0x00000000     0xF8C, 0x00000000     
0xF90, 0x00000000     0xF94, 0x80000000     0xF98, 0x00000000     0xF9C, 0x2F003000     
0xFA0, 0x30002F00     0xFA4, 0x2F002F00     0xFA8, 0x2E003100     0xFAC, 0x2F000000     
0xFB0, 0x00000003     0xFB4, 0x1F1C1C1E     0xFB8, 0x0E1D1E0E     0xFBC, 0x1F1D0F0F     
0xFC0, 0x1E1F1E1D     0xFC4, 0x1F1E1C1E     0xFC8, 0x1C1D1E1D     0xFCC, 0x1F1F1E1F     
0xFD0, 0x1F1F1F1D     0xFD4, 0x1F1D1A1D     0xFD8, 0x1C1E1C1B     0xFDC, 0x1F1D1A1D     
0xFE0, 0x1D1F1D1C     0xFE4, 0x1F0D1B0D     0xFE8, 0x1D1D1C1B     0xFEC, 0x1F201D20     
0xFF0, 0x1F22201E     0xFF4, 0x1F1E1A1D     0xFF8, 0x1C1E1C1B     0xFFC, 0x1F003340 
0 Kudos
Reply

614 Views
June_Lu
NXP TechSupport
NXP TechSupport

Thanks, we have frwyls1046a which could pass the validation.

Please find the video attached to QCVS error report(HTML format) .

0 Kudos
Reply