DDR4 and ECC on LS1046

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR4 and ECC on LS1046

2,498 Views
Filippo
Contributor III

Hi all,

I'm approaching an LS1046 design, and I would like to use a non-ECC DDR4.

On the reference design ( sch-29142 ) there is the socket for a 288 pin ecc ddr4 dimm.

Can I avoid to use ECC, so using a 260 pin ddr4 module ?

Regards

Filippo

Labels (1)
0 Kudos
Reply
2 Replies

2,196 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes you can to use a non-ECC DDR4 memory. The DDR ECC is enabled in the DDR_SDRAM_CFG register.  

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,165 Views
atrqua
Contributor I

Have u met  a  NOTICE about DDR :NOTICE: UDIMM M4DS-AGS1QC0J-BE82  when boot LS1046 ?

Thank u

0 Kudos
Reply