Hi all,
I'm approaching an LS1046 design, and I would like to use a non-ECC DDR4.
On the reference design ( sch-29142 ) there is the socket for a 288 pin ecc ddr4 dimm.
Can I avoid to use ECC, so using a 260 pin ddr4 module ?
Regards
Filippo
Have a great day,
Yes you can to use a non-ECC DDR4 memory. The DDR ECC is enabled in the DDR_SDRAM_CFG register.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Have u met a NOTICE about DDR :NOTICE: UDIMM M4DS-AGS1QC0J-BE82 when boot LS1046 ?
Thank u